Bootloader UART: NACK to Write Command when try to write data to valid RAM memory addresses
- 3 replies
- 2235 views
To whom it may concern:
We are currently developing a wearable devices, which is running on a STM32L031. In Bootloader mode, while I am trying to write data to vaild RAM address(0x20001F00), it returns NACK. Every step is followed instruction, but it just won't work on STM32L031 platform. Then I ran the same code try to write STM32H750 address and success(write to 0x20004108). I think I can't solve this on my own, Please help. :crying_face:
I've attached a logic analyzer photo includes UART data, first line is host side, second one is device side.(See attachments)
By the way( Another question), I have two identical MCU(let's call master and slave) which connected with UART, I want to copy master's firmware to slave through UART bootloader. The hardware connection is correct and the bootloader can be entered. In this write process, on every stage slave returns ACK, but after reboot the code doesn't run. Then I dumped slave's hex file by SWD and compared with master's one using hex comparson tool, then I found many differences( about 30% is wrong). Shoud I erase flash before I write? Is there any host code example? Any suggestion would help. My MCU is STM32L031. The waveforms seen with the oscilloscope are quite good.
Application note used: AN3155 ver.16, AN2606 ver.59
MCU : STM32L031E6Y6DTR
UART info : baud rate 62500(because HSI is 32M, I've already tried 115200, 9600), parity even, 8bits , 1 stop bit.
For unknown reason I can't attach photo to context or upload, I have to upload a docx file. Sorry for unconvient.