Skip to main content
DChen.3
Associate
Jul 17, 2020 7:02 AM UTC
Question

Bootloader command set trouble in write memory command set

I try use the boot loader command set.

I follow the AN3155 datasheet to use , but i meet a trouble, i can't write bytes over 4 bytes. below is my set step

  1. send cmd host -> 31 CE / device-> 79
  2. send address+checksum host->08 00 00 00 08 / device->79
  3. send number+checksum host->04 00 04 00 20 00 20 / device->79

but if I want to write more byte or one bin file , then device all response 1F(NACK)

example :

host-> 0c 00 04 00 20 a9 8b 00 00 03 8e 00 00 00 00 /device ->1F

send 128 bytes host-> 80 00 04 00 20..............80 00 00 00 00 /device->1F

Could you talk me where is error? thank you

This topic has been closed for replies.

2 replies

TDK
Jul 17, 2020 1:04 PM UTC

> 04 00 04 00 20 00 20

This writes 5 bytes, not 4.

> 0c 00 04 00 20 a9 8b 00 00 03 8e 00 00 00 00

This writes 13 bytes and the checksum is wrong.

"If you feel a post has answered your question, please click ""Accept as Solution""."
DChen.3
DChen.3Author
Associate
Jul 22, 2020 3:11 AM UTC

Please tell me how to cal the checksum?? and the data string checksum is ?