Skip to main content
EmirhanS
Associate
July 13, 2025
Question

Bootloader/BootROM Cannot Execute App Code on SDRAM Address

Hello,
I am currently working on a bootloader code. I successfully managed to execute the app code by copying to the RAM address (0x20000000). However, whenever I try to copy the app code to SDRAM (0xC0000000) instead of RAM, bootloader never executes the app code. 

In the linker script file of my app, I follow the same process with the "RAM Version" of the code: I used SDRAM address for all sectors (.data, .text, .bss...). 

My jump code is basically like:

 uint32_t app_sp = *((volatile uint32_t*)APP_SDRAM_ADDRESS);
 uint32_t app_pc = *((volatile uint32_t*)(APP_SDRAM_ADDRESS + 4));
 SCB->VTOR = APP_SDRAM_ADDRESS;
 __set_MSP(app_sp);
 ((void (*)(void))app_pc)();

 
Thanks.

This topic has been closed for replies.

3 replies

MM..1
Super User
July 13, 2025

From where you have idea this works? Minimum is special init code, that block reinit external memorry...

EmirhanS
EmirhanSAuthor
Associate
July 13, 2025

Hi,
I appreciate your answer. Maybe it is because of the lack of my experience but I did not understand your answer well:
"that block reinit external memorry."
Thanks.

MM..1
Super User
July 13, 2025

Simply internal RAM works after MCU is powered, but FMC require sw init, and this init is i hope once in your bootlodaer code, but if exist in app code too = reinit = fail run same code in SDRAM

Try chatgpt ask "stm32f7 condition to run code in sdram"