bin file is gigantic, hex and elf files are normal, when defining a section of RAM in STM32F765VITx
- 6 replies
- 5233 views
I'm trying to define a region of RAM for storing debug information that can persist following a reset (DEBUG_RAM). I'd like to put variables in a section (.debug_ram) that are stored in the DEBUG_RAM memory such its usage properly displays in the Build Analyzer.
When I do this my elf and hex files are a normal size, 1.3MB and 15kB respectively. My bin files, however, are 393MB. Unfortunately the company I work for has standardized on bin files, particularly for their bootloader software.
I have attached my modified linker file (renamed STM32F765VITX_FLASH.ld.c so that it can be attached to the forum) and main.c where I locate the debug_ram_test variable in the in the .debug_ram section. When I build the build analyzer window correctly shows that 6.25% of the DEBUG_RAM region is used.
If I use a bin-to-hex utility to convert the bin file I see it's almost all data records with all of the data equal to zero, interspersed with Extended Linear Address records outside the range for the FLASH for the MCU. Here is an example:
:10FFC000000000000000000000000000000000000000000000000000000000000000000031
:10FFD000000000000000000000000000000000000000000000000000000000000000000021
:10FFE000000000000000000000000000000000000000000000000000000000000000000011
:10FFF000000000000000000000000000000000000000000000000000000000000000000001
:01000004FF0FED
:100000000000000000000000000000000000000000000000000000000000000000000000F0
:100010000000000000000000000000000000000000000000000000000000000000000000E0
:100020000000000000000000000000000000000000000000000000000000000000000000D0
:100030000000000000000000000000000000000000000000000000000000000000000000C0
I'm really hoping that I'm doing something dumb that I can fix, but I've done this on lots of projects before and probably never noticed because I only used hex files.