Skip to main content
james4452
Associate
Sep 30, 2026 3:44 AM UTC
Solved

Best way to handle SDRAM + LTDC together on STM32H7 without cache artifacts?

I'm working on an STM32H743-based project driving a parallel LCD through LTDC, with the framebuffer sitting in external SDRAM via FMC. I keep running into intermittent display corruption that I suspect is cache-related, since the M7 core has D-Cache enabled by default.

What's the recommended approach for setting up the MPU region for the framebuffer — mark the whole SDRAM region as non-cacheable, or is it better to keep caching enabled and handle cache maintenance manually (SCB_CleanDCache_by_Addr) around framebuffer writes? Curious what's worked best for people running LTDC + SDRAM at higher resolutions/refresh rates without a performance hit.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 30, 2026 8:26 AM UTC

Hello,

AN4861 “Introduction to LCD-TFT display controller (LTDC) for STM32 MCUs” / especially the section 5.6 Special recommendations for Cortex M7 (STM32F7/H7) and Cortex M55 (STM32N6).

1- Need to ensure to prevent any CM7 speculative access to an invalid address region to prevent any loss of display performance. Read also this article:

2- Ensure the data coherency. Read “MPU and cache policy configuration” section in the same AN4861

Hope that helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

MM..1
Super User
Sep 30, 2026 4:09 AM UTC
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 30, 2026 8:26 AM UTC

Hello,

AN4861 “Introduction to LCD-TFT display controller (LTDC) for STM32 MCUs” / especially the section 5.6 Special recommendations for Cortex M7 (STM32F7/H7) and Cortex M55 (STM32N6).

1- Need to ensure to prevent any CM7 speculative access to an invalid address region to prevent any loss of display performance. Read also this article:

2- Ensure the data coherency. Read “MPU and cache policy configuration” section in the same AN4861

Hope that helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.