Skip to main content
Associate II
Dec 20, 2024 3:47 PM UTC
Solved

Best practices for I2C driver architecture

Hi,

I want to use a single low-level module to handle up to three I2C buses at the same time using the HAL library and using the interrupt for all communications with the relative callback. Is it possible to use a single write/read/callback function for all transactions on all three buses at the same time. Are there any problems if the callback is interrupted to handle another interrupt of another I2C bus with higher priority?

Best regards,

Domenico

This topic has been closed for replies.
TDK
TDKBest answer
Dec 22, 2024 1:44 AM UTC

Should be no problems doing this with HAL. Get one instance working first and it should be straightfoward to move to multiple. They will all use different handles.

I2C interrupts pre-empting should not cause issues. However I2C is so slow compared to interrupt execution speed that I'd set them all at the same priority.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

Karl Yamashita
Principal
Dec 20, 2024 10:55 PM UTC

As long as you have different data buffer or structure for each bus then you will be fine. But if you are sharing the same data buffer, then you'll get conflicts as 1 of the bus will over write the other bus data.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
TDK
TDKBest answer
Dec 22, 2024 1:44 AM UTC

Should be no problems doing this with HAL. Get one instance working first and it should be straightfoward to move to multiple. They will all use different handles.

I2C interrupts pre-empting should not cause issues. However I2C is so slow compared to interrupt execution speed that I'd set them all at the same priority.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
Dec 30, 2024 10:47 AM UTC

Ok, thanks for your solution.