Skip to main content
Associate II
May 22, 2026
Question

Best ethernet config for benchamrking on STM32H753

Hello, I hope you are doing well.

I am currently working on benchmarking the Ethernet communication interface on an STM32H753 Nucleo board.

My setup involves sending data from a Python script to the STM32, where the data is encrypted, and then sent back. This allows me to measure the RTT and overall throughput.

I initially used Mongoose, but I encountered several issues:

  • With UDP, I cannot reliably send more than ~1500 bytes, since larger packets get fragmented or dropped.
  • TCP works correctly, but the throughput varies significantly depending on payload size. For example:
    • ~2.7 MiB/s for 1400-byte payloads
    • ~7 MiB/s for 10240-byte payloads

I would like to know:

  1. What is the best networking stack or library for STM32 to achieve better performance and properly handle UDP large payloads?
  2. Given that Ethernet is 100 Mbps in my case, I am not reaching near-theoretical throughput even without encryption. Is this because I am measuring not only transmission time but also packet handling, buffering, and processing overhead (e.g., encryption, stack processing)? Is this assumption correct?



Thank you  

2 replies

mbarg.1
Senior III
May 22, 2026

Well. I find your question very nice.

We faced the similar problem - we wanted to have a reliable websockets conenction with a bunch (<16) of clients on IP4 and IP6 while flooding the interface with classicl flood of sync.

We were unable to get both freertos and azure stable - our fault probably - and we decided to move to a proprietary solution built on top of azure rtos and STM HAL without netxDuo.

If you mind, I can share the code, but be aware we can do only if you are based in a non-conflict area.

Let me know.

g2f1Author
Associate II
May 22, 2026

Hello, what you mean by non-conflict area?