Skip to main content
CWern.1
Associate II
Jun 9, 2021 9:36 AM UTC
Question

Behavior with _LOW_POWER

Hi everyone,

I am working on an USB-PD source that is battery powered.

To make use of the low power features, I defined _LOW_POWER.

When this is defined, I get a problem in connection with eletronically marked cables (EMC). Non-EMC cables work fine.

The system will get stuck in the state currentHWcondition "HW_PwrCable_NoSink_Attachment".

I investigated the issue and found that the system works perfectly once I commented the following lines in usbpd_cad_hw_if.c related to _LOW_POWER

uint32_t CAD_StateMachine(uint8_t PortNum, USBPD_CAD_EVENT *pEvent, CCxPin_TypeDef *pCCXX)
{
 CAD_HW_HandleTypeDef *_handle = &CAD_HW_Handles[PortNum];
 uint32_t _timing = CAD_DEFAULT_TIME;
 
 /* set by default event to none */
 *pEvent = USBPD_CAD_EVENT_NONE;
 
 if (USBPD_TRUE == Ports[PortNum].params->PE_SwapOngoing)
 {
 return _timing;
 }
 
 if (_handle->CAD_ErrorRecoveryflag == USBPD_TRUE)
 {
 /* Force the state error recovery */
 _handle->CAD_ErrorRecoveryflag = USBPD_FALSE;
 _handle->cstate = USBPD_CAD_STATE_ERRORRECOVERY;
#if defined(_TRACE)
 USBPD_TRACE_Add(USBPD_TRACE_CAD_LOW, PortNum, (uint8_t)_handle->cstate, NULL, 0);
#endif /* _TRACE */
 }
 
 switch(_handle->cstate)
 {
 case USBPD_CAD_STATE_RESET:
 {
//#if !defined(_LOW_POWER) && !defined(USBPDM1_VCC_FEATURE_ENABLED)
		//DBG
 LL_UCPD_EnableIT_TypeCEventCC2(Ports[PortNum].husbpd);
 LL_UCPD_EnableIT_TypeCEventCC1(Ports[PortNum].husbpd);
//#endif /* !_LOW_POWER */
 if( 0 == PortNum)
 {
 UCPD_INSTANCE0_ENABLEIRQ;
 }
#if USBPD_PORT_COUNT > 1
 else
 {
 UCPD_INSTANCE1_ENABLEIRQ;
 }
#endif /* USBPD_PORT_COUNT > 1 */
#if defined(_DRP) || defined(_ACCESSORY_SNK)
 _handle->CAD_tToggle_start = HAL_GetTick();
#endif /* _DRP || _ACCESSORY_SNK */
 _handle->cstate = USBPD_CAD_STATE_DETACHED;
 break;
 }
void CAD_Check_HW_SRC(uint8_t PortNum)
{
#if !defined(_RTOS)
 uint32_t CC1_value_temp, CC2_value_temp;
#endif /* !_RTOS */
 CAD_HW_HandleTypeDef *_handle = &CAD_HW_Handles[PortNum];
 /* done to prevent code optimization issue with GCC */
 uint32_t CC1_value, CC2_value;
 
 /*
 ----------------------------------------------------------------------------
 | ANAMODE | ANASUBMODE[1:0] | Notes | TYPEC_VSTATE_CCx[1:0] |
 | | | | 00 | 01 | 10 | 11 |
 ----------------------------------------------------------------------------
 | 0: Source | 00: Disabled |Disabled N/A | NA |
 | | 01: Default USB Rp| |vRaDef|vRdDef|vOPENDef| |
 | | 10: 1.5A Rp | |vRa1.5|vRd1.5|vOPEN1.5| NA |
 | | 11: 3.0A Rp | |vRa3.0|vRd3.0|vOPEN3.0| NA |
 -----------------------------------------------------------------------------
 | 1: Sink | | |xx vRa|vRdUSB| vRd1.5 |vRd3.0|
 -----------------------------------------------------------------------------
 */
//DBG
//#ifdef _LOW_POWER
// /* Enable type C state machine */
// CLEAR_BIT(Ports[PortNum].husbpd->CR, UCPD_CR_CC1TCDIS | UCPD_CR_CC2TCDIS);
 
// for(int32_t index=0; index < 200/2; index++){ __DSB();};
//#endif /* _LOW_POWER */
 
 CC1_value = (Ports[PortNum].husbpd->SR & UCPD_SR_TYPEC_VSTATE_CC1) >> UCPD_SR_TYPEC_VSTATE_CC1_Pos;
 CC2_value = (Ports[PortNum].husbpd->SR & UCPD_SR_TYPEC_VSTATE_CC2) >> UCPD_SR_TYPEC_VSTATE_CC2_Pos;
//DBG
//#ifdef _LOW_POWER
// /* Disable the C state machine */
// SET_BIT(Ports[PortNum].husbpd->CR, UCPD_CR_CC1TCDIS | UCPD_CR_CC2TCDIS);
//#endif /* _LOW_POWER */
 

Is this a known issue or am I using the code wrong in some other place?

Thanks,

Christian

This topic has been closed for replies.

11 replies

Yohann M.
ST Employee
Jun 11, 2021 6:59 AM UTC

Dear Christian

This issue is not a known issue. could you please provide further information? How do you start from? X-CUBE-TCPP with SINK LPM application? FW G0 Package?

Anyway, I will raise a ticket internally to track this issue and come back to you.

Regards,

Yohann

CWern.1
CWern.1Author
Associate II
Jun 11, 2021 9:06 AM UTC

Hi Yohann,

I am using a STM32G071GBN. I started from the CubeMX version 6.2 with the G0 package version 1.4. I created a Source application.

For the low power handling I looked up the example project for the STM32G081b-Eval "USB-PD_Provider_1Port". And I am using the non-Os implementation.

Thanks,

Christian

Yohann M.
ST Employee
Jun 11, 2021 9:26 AM UTC

Thanks for your feedback!

In meanwhile, did you have a look at the application we delivered for Low Power in sink mode?

x-cube-tcpp/Projects/NUCLEO-G071RB/Applications/USB_PD/USBPDM1_Sink_LPM at main · STMicroelectronics/x-cube-tcpp · GitHub

Yohann

CWern.1
CWern.1Author
Associate II
Jul 1, 2021 12:58 PM UTC

Yes I did have a look at your example. I don't see a difference in the middleware files, aside from it being a sink and I have a source application. So I don't know how comparable the two projects are.

Did you have any luck replicating this behavior?

Christian

CWern.1
CWern.1Author
Associate II
Sep 23, 2021 10:51 AM UTC

Dear Yohann,

I tested the file you supplied with the old version 3.2 and the new 4.0.0 of the USB-PD library. Unfortunately no luck with both. Problem still persists.

Yohann M.
ST Employee
Sep 27, 2021 6:39 AM UTC

Dear Christian,

Is it possible to provide the project to this thread?

regards,

Yohann

CWern.1
CWern.1Author
Associate II
Oct 14, 2021 11:03 AM UTC

Dear Yohann,

yes I can share it with you. Is there any way I can get it to you?