Skip to main content
Associate
Jun 6, 2024 4:26 AM UTC
Question

B-U585I-IOT02A- mxchip/nx_driver_framework.c: error This file is included by the drive

I am trying to develop the Nx_TCP_Echo_Server example from scratch using library generation. While integrating MX_WIFI, I am encountering a compilation error related to NetX Duo and the Wi-Fi driver.

 

Spoiler

/Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:  error: #error This file is included by the driver source, not compiled directly.

 #error This file is included by the driver source, not compiled directly

/Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:27:2: error: #error This file is included by the driver source, not compiled directly. #error This file is included by the driver source, not compiled directly.

@Guillaume K 

This topic has been closed for replies.

3 replies

Guillaume K
ST Employee
Jun 7, 2024 7:55 AM UTC

Hi

It's difficult to answer without knowing all the details of your project.

what do you mean by "using library generation" ?

As said in the error, nx_driver_framework.c must not be present in the IDE project file. It must not be compiled directly by the IDE.

It is included in nx_driver_emw3080.c.

What IDE are you using ? STM32CubeIDE ?

zibAuthor
Associate
Jun 7, 2024 12:13 PM UTC

trying to develop athe Mxchip EMW380 WiFi module with the B-U585I-IOT02A board, using ThreadX RTOS and NetX Duo,


integrating temperature and barometric sensors (ISM330DHCX and LPS22HH) using I2C and establishing a WiFi connection via SPI2

 and generated from  .ioc file 

https://wiki.stmicroelectronics.cn/stm32mpu/wiki/Introduction_to_NETXDUO

  above example i have added  driver file of  mx_chip add to   project file system and  added  the path for newly added file in  C/C++m  build setups  , tree of  project file  added
   and  copied the  app_thread.c .h and app_netx.c .h  and other file from Nx_TCP_Echo_Server, to   project  file system

while compiling  facing issue from 

 

./Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:27:2: error: #error This file is included by the driver source, not compiled directly.

27 | #error This file is included by the driver source, not compiled directly.

| ^~~~~

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:33:1: error: unknown type name 'NX_DRIVER_INFORMATION'

33 | NX_DRIVER_INFORMATION nx_driver_information;

| ^~~~~~~~~~~~~~~~~~~~~

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c: In function 'nx_driver_framework_entry_default':

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:258:48: error: 'NX_DRIVER_ERROR' undeclared (first use in this function); did you mean 'NX_CALLER_ERROR'?

258 | driver_req_ptr -> nx_ip_driver_status = NX_DRIVER_ERROR;

| ^~~~~~~~~~~~~~~

| NX_CALLER_ERROR

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:258:48: note: each undeclared identifier is reported only once for each function it appears in

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c: In function 'nx_driver_interface_attach':

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:312:24: error: request for member 'nx_driver_information_interface' in something not a structure or union

312 | nx_driver_information.nx_driver_information_interface = driver_req_ptr -> nx_ip_driver_interface;

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c: In function 'nx_driver_initialize':

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:378:24: error: request for member 'nx_driver_information_ip_ptr' in something not a structure or union

378 | nx_driver_information.nx_driver_information_ip_ptr = NX_NULL;

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:381:24: error: request for member 'nx_driver_information_state' in something not a structure or union

381 | nx_driver_information.nx_driver_information_state = NX_DRIVER_STATE_NOT_INITIALIZED;

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:381:55: error: 'NX_DRIVER_STATE_NOT_INITIALIZED' undeclared (first use in this function)

381 | nx_driver_information.nx_driver_information_state = NX_DRIVER_STATE_NOT_INITIALIZED;

| ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:384:24: error: request for member 'nx_driver_information_packet_pool_ptr' in something not a structure or union

384 | nx_driver_information.nx_driver_information_packet_pool_ptr = ip_ptr -> nx_ip_default_packet_pool;

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:387:24: error: request for member 'nx_driver_information_deferred_events' in something not a structure or union

387 | nx_driver_information.nx_driver_information_deferred_events = 0;

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:412:26: error: request for member 'nx_driver_information_ip_ptr' in something not a structure or union

412 | nx_driver_information.nx_driver_information_ip_ptr = driver_req_ptr -> nx_ip_driver_ptr;

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:422:26: error: request for member 'nx_driver_information_state' in something not a structure or union

422 | nx_driver_information.nx_driver_information_state = NX_DRIVER_STATE_INITIALIZED;

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:422:57: error: 'NX_DRIVER_STATE_INITIALIZED' undeclared (first use in this function)

422 | nx_driver_information.nx_driver_information_state = NX_DRIVER_STATE_INITIALIZED;

| ^~~~~~~~~~~~~~~~~~~~~~~~~~~

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:430:45: error: 'NX_DRIVER_ERROR' undeclared (first use in this function); did you mean 'NX_CALLER_ERROR'?

430 | driver_req_ptr -> nx_ip_driver_status = NX_DRIVER_ERROR;

| ^~~~~~~~~~~~~~~

| NX_CALLER_ERROR

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c: In function 'nx_driver_enable':

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:484:28: error: request for member 'nx_driver_information_state' in something not a structure or union

484 | if (nx_driver_information.nx_driver_information_state < NX_DRIVER_STATE_INITIALIZED)

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:484:59: error: 'NX_DRIVER_STATE_INITIALIZED' undeclared (first use in this function)

484 | if (nx_driver_information.nx_driver_information_state < NX_DRIVER_STATE_INITIALIZED)

| ^~~~~~~~~~~~~~~~~~~~~~~~~~~

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:487:45: error: 'NX_DRIVER_ERROR' undeclared (first use in this function); did you mean 'NX_CALLER_ERROR'?

487 | driver_req_ptr -> nx_ip_driver_status = NX_DRIVER_ERROR;

| ^~~~~~~~~~~~~~~

| NX_CALLER_ERROR

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:492:28: error: request for member 'nx_driver_information_state' in something not a structure or union

492 | if (nx_driver_information.nx_driver_information_state >= NX_DRIVER_STATE_LINK_ENABLED)

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:492:60: error: 'NX_DRIVER_STATE_LINK_ENABLED' undeclared (first use in this function); did you mean 'NX_IP_INTERFACE_LINK_ENABLED'?

492 | if (nx_driver_information.nx_driver_information_state >= NX_DRIVER_STATE_LINK_ENABLED)

| ^~~~~~~~~~~~~~~~~~~~~~~~~~~~

| NX_IP_INTERFACE_LINK_ENABLED

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:513:26: error: request for member 'nx_driver_information_state' in something not a structure or union

513 | nx_driver_information.nx_driver_information_state = NX_DRIVER_STATE_LINK_ENABLED;

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c: In function 'nx_driver_disable':

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:578:28: error: request for member 'nx_driver_information_state' in something not a structure or union

578 | if (nx_driver_information.nx_driver_information_state != NX_DRIVER_STATE_LINK_ENABLED)

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:578:60: error: 'NX_DRIVER_STATE_LINK_ENABLED' undeclared (first use in this function); did you mean 'NX_IP_INTERFACE_LINK_ENABLED'?

578 | if (nx_driver_information.nx_driver_information_state != NX_DRIVER_STATE_LINK_ENABLED)

| ^~~~~~~~~~~~~~~~~~~~~~~~~~~~

| NX_IP_INTERFACE_LINK_ENABLED

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:581:45: error: 'NX_DRIVER_ERROR' undeclared (first use in this function); did you mean 'NX_CALLER_ERROR'?

581 | driver_req_ptr -> nx_ip_driver_status = NX_DRIVER_ERROR;

| ^~~~~~~~~~~~~~~

| NX_CALLER_ERROR

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:602:26: error: request for member 'nx_driver_information_state' in something not a structure or union

602 | nx_driver_information.nx_driver_information_state = NX_DRIVER_STATE_INITIALIZED;

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:602:57: error: 'NX_DRIVER_STATE_INITIALIZED' undeclared (first use in this function)

602 | nx_driver_information.nx_driver_information_state = NX_DRIVER_STATE_INITIALIZED;

| ^~~~~~~~~~~~~~~~~~~~~~~~~~~

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c: In function 'nx_driver_packet_send':

 

| ^

../Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.c:1246:23: error: 'NX_DRIVER_ETHERNET_IP' undeclared (first use in this function)

1246 | if ((packet_type == NX_DRIVER_ETHERNET_IP) || (packet_type == NX_DRIVER_ETHERNET_IPV6))

| ^~~~~~~~~~~~~~~~~~~~~

 

| ^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

make: *** [Middlewares/ST/netxduo/common/drivers/wifi/mxchip/subdir.mk:25: Middlewares/ST/netxduo/common/drivers/wifi/mxchip/nx_driver_framework.o] Error 1

make: *** Waiting for unfinished jobs....

 

 

 

Guillaume K
ST Employee
Jun 7, 2024 2:54 PM UTC

Do you confirm you are using STM32CubeIDE to compile ?

The link you mention is wiki.stmicroelectronics.cn. I suggest you use wiki.st.com

The link points to a wiki that talks about stm32mpu. If you are working with a B-U585I-IOT02A, you should get information from stm32mcu wiki.

If you are using STM32CubeIDE , maybe you have used a project with "generate at root" option. In this mode, all the source files are installed in same folder as STM32CubeIDE .project and .cproject files, and in sub directory.

By default, STM32CubeIDE compiles all the source files (*.c files) that it finds near .cproject and .project and in sub directories.

The problem is that nx_driver_framework.c is in Middlewares/ST/netxduo/common/drivers/wifi/mxchip. It will be compiled automatically.

One solution is : if you used STM32CubeMX, change the project setting to generate STM32CubeIDE project but without "generate at root" option. It will create the STM32CubeIDE project files .project and .cproject in a STM32CubeIDE/ directory. The sources will be referenced with links in .project file. The problem is that it changes all your project.

Another solution is to rename nx_driver_framework.c as nx_driver_framework.h and change the #include line in nx_driver_emw3080.c to use the new name.