Skip to main content
Keyur Thumar
Associate III
Jun 23, 2022 5:01 AM UTC
Question

B-L475E-IOT01A USB DFU is stuck in different states.

I am using B-L475E-IOT01A (STM32L475VGTx) dev kit and this article for DFU and I am getting following issue.

Sequence of process I do is as below.

  • Erase the whole flash.
  • Flash the bootloader created based on above video.
  • Make a DFU using DfuSe Tool and It works.

But when I want to upgrade the device again with DfuSe Tool, DFU process stuck or gives me error. Please see below screenshot.

0693W00000NsWVVQA3.png0693W00000NsWVfQAN.pngUpgrade file is simple LED blinking application. It works when I do the DFU first time. But for upcoming DFU does not work.

Can anyone please help me out here ?

This topic has been closed for replies.

12 replies

Keyur Thumar
Associate III
Jul 1, 2022 5:48 AM UTC

@Mike_ST​  Thank you for resoultion and explanation.

I have done changes as you suggested and it worked. :grinning_face:

I have gone through the AN3156 but couldn't get an idea of why the workaround you suggested is worked or what is incomplete in my DFU protocol implementation.

Can you please elaborate ? It would be great help for me.

Mike_ST
ST Technical Moderator
Jul 1, 2022 7:42 AM UTC

This implementation is only an example and is only deleting 1 page of flash memory before programming.

So it would work for small binaries (2KB max) and that is why deleting more flash pages helps.

So you have to understand it and adapt it for your needs.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.