Skip to main content
Bhong.11
Visitor II
September 1, 2025
Question

AZURE RTOS PESSRAE certification

  • September 1, 2025
  • 2 replies
  • 435 views

Hello. This is HPNRT Co., Ltd. We are currently in the process of PESSRAE certification for our escalator auxiliary brake, a component that requires certification. We are developing the system using the STM32H743 MPU and plan to use Azure RTOS as the operating system. We were informed that the development and sales of Azure RTOS are free, but we need the Certificate Document for PESSRAE certification. Could you please assist us with this? Does the PESSRAE-related process require a separate contract? We would also appreciate it if you could provide us with the procedure for obtaining Azure RTOS PESSRAE certification and the email address of the relevant department at your company.

Thank you.

This topic has been closed for replies.

2 replies

ST Technical Moderator
September 2, 2025

Hello @Bhong.11 

I reported your question internally and will get back to you as soon as possible. 

Internal ticket number: 216729 (This is an internal tracking number and is not accessible or usable by customers).

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
ST Technical Moderator
September 26, 2025

Hello @Bhong.11 

Azure RTOS doesn't have dedicated PESSRAE certification
Azure RTOS has functional safety certifications:
- IEC 61508-3:2010; clause 7.4.2.12, route 3S
- IEC 62304:2015
- ISO 26262-8:2018; clause 12
- EN 50128:2011; clause 7.3.4.7
You need to join the ThreadX Alliance hosted by the Eclipse Foundation to get access to the safety artefacts. You can join Frequently Asked Questions (FAQ) | ThreadX Alliance | The Eclipse Foundation to get more information.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om