Skip to main content
Associate
January 5, 2026
Solved

Audio How to play audio files using STM32F103C8T6

Hi,
I want to design a voice announcement system using the STM32F103C8T6.
My requirement is to Load WAV audio files from an SD card and play them using the STM32, without using any external DAC.

I would like guidance on how to start the project using STM32CubeMX / STM32CubeIDE, including:

  • Peripheral configuration in CubeMX

  • Audio playback method without a DAC (for example, PWM-based audio)

  • Basic coding structure to read WAV files from an SD card and play them

Any help or reference projects would be greatly appreciated.

 

I have design hardware also here attachment is there please go through it ...Thank you 

 

 

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
January 6, 2026

@itrajusankar The examples given by @MOBEJ refer to an external audio DAC, which would also be possible with an STM32F103. However, apart from the schematics, you have not provided many details so far, neither that it is an genuine STM32F103 and not one of the many counterfeits, nor the expected maximum audio frequency, nor an explanation of what you mean by ‘not as good as expected’ in the result.

We can only speculate at this point and assume that you are using TIM4 as a PWM output on PB6 and PB8, correct?
I must also assume that you are generating an internal frequency of 72MHz from the HSE=8MHz. Your low-pass filter of 1k+100nF, which you have on each of the two PWM outputs, has a cut-off frequency of 1591Hz, which could be suitable for subwoofers at best. For reasonably good audio quality (which also needs to be defined first), I assume a minimum PWM resolution of 14 bits. With these parameters, we can already estimate the result: 72MHz/16384 ~ 4394Hz, which is extremely attenuated by the low-pass filter – this cannot produce a meaningful result.

Regards
/Peter

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

15 replies

Peter BENSCH
ST Technical Moderator
January 5, 2026

Welcome @itrajusankar, to the community!

If your STM32F103C8T6 is on a so called Blue Pill, it is most likely not a device from STMicroelectronics but an illegal counterfeit, so you would need to contact its manufacturer.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
January 6, 2026

HI Peter Thank you for your quick replay We are not using Blue Pill board We have design our customized board. Please find schematic thank you.

Andrew Neil
Super User
January 5, 2026

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

 


@itrajusankar wrote:

using the STM32F103C8T6.


As @Peter BENSCH said, if that's on a Blue Pill, then prepare for a bumpy ride... !

For a better experience, I would strongly suggest that you get a Nulceo-F103 instead.

 

Do you already have experience with STM32? and/or any other microcontroller(s)?

If not, then it would be better to start with some basics first.

 

As always, the secret is to break down your project into manageable parts; eg,

  • Using PWM
  • Using FatFs
  • Decoding a .WAV file

ST provide examples for the first two - especially if you use an ST board.

 


@itrajusankar wrote:

I have design hardware also here attachment is there please go through it .


You forgot the attachment?

Did you study the Application note AN2586, "Getting started with STM32F10xxx hardware development" ?

And other documentation:

https://www.st.com/en/microcontrollers-microprocessors/stm32f103c8.html#documentation

 

Again,  I would strongly suggest that you start on a known-good board (eg, Nucleo) before adding the uncertainties of unverified hardware!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
January 6, 2026

Hi Andrew,

Thank you for your quick reply.

We have already designed our custom board, and it is working fine. We also have some experience with the STM32F103C8T6. However, this is our first project involving audio-related applications.

We are able to get voice output, but the audio clarity is not as good as we expected. Kindly guide us with some example code or reference implementation to help improve the audio quality.

Thank you for your support.

 
Ozone
Principal
January 5, 2026

> ... without using any external DAC.

That's fine - but you still need to tell us how you want to output those WAV files, and in a way they remain comprehensible.
A lot depends on that.

> - Basic coding structure to read WAV files from an SD card and play them

Just use a file system like FatFS.
With that, more generic WAV file examples will do.

Select an appropriate library for decoding WAV files that can be ported to a CM3, or for which already ports exist.
Decoding RIFF files "by hand" (with you own code) is less than trivial, and would consume a lot of time and effort.

Andrew Neil
Super User
January 5, 2026

As @Ozone suggests, decoding a WAV file may be non-trivial.

The format is well-documented and widely-used; eg, https://en.wikipedia.org/wiki/WAV

You might be able to simplify your implementation by restricting yourself to just a certain specific type of WAV file.

Or maybe just use a simple binary format instead?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Ozone
Principal
January 5, 2026

> Or maybe just use a simple binary format instead?

Which is what I would probably do.
Convert them to simple binary files of fixed format (probably signed 8-bit) and sampling frequency, and store them either in SD card files of fixed names, or in Flash.
PC-based libraries make reading and decoding WAV a relatively trivial task, so even writing such a converter tool would not consume much time.

MOBEJ
ST Employee
January 5, 2026

Hello @itrajusankar , 

You can find an audio example using I2S with DMA in the I2S_Audio example  on GitHub. This example demonstrates how to play an audio file with an external codec on the STM32F1xx board via the I2S peripheral using DMA transfers.

Additionally, you can refer to the BSP example in the sub-demo named "AUDIO PLAY". This example shows how to play, pause, resume, and adjust the volume (from 50% to 100%) of audio playback using the Key or Joystick buttons.

You can adapt and deploy these examples to your own STM32 device by modifying the peripheral settings and pin configurations accordingly.
Br

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
January 6, 2026

Hi

 MOBEJ

Thank you for your quick reply.

We have already designed our custom board, and it is working fine. We also have some experience with the STM32F103C8T6. However, this is our first project involving audio-related applications.

We are able to get voice output, but the audio clarity is not as good as we expected. Kindly guide us with some example code or reference implementation to help improve the audio quality.

Thank you for your support.

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
January 6, 2026

@itrajusankar The examples given by @MOBEJ refer to an external audio DAC, which would also be possible with an STM32F103. However, apart from the schematics, you have not provided many details so far, neither that it is an genuine STM32F103 and not one of the many counterfeits, nor the expected maximum audio frequency, nor an explanation of what you mean by ‘not as good as expected’ in the result.

We can only speculate at this point and assume that you are using TIM4 as a PWM output on PB6 and PB8, correct?
I must also assume that you are generating an internal frequency of 72MHz from the HSE=8MHz. Your low-pass filter of 1k+100nF, which you have on each of the two PWM outputs, has a cut-off frequency of 1591Hz, which could be suitable for subwoofers at best. For reasonably good audio quality (which also needs to be defined first), I assume a minimum PWM resolution of 14 bits. With these parameters, we can already estimate the result: 72MHz/16384 ~ 4394Hz, which is extremely attenuated by the low-pass filter – this cannot produce a meaningful result.

Regards
/Peter

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.