Skip to main content
ben5en
Associate II
Aug 4, 2021 2:10 PM UTC
Solved

Are there plans for CAN support in open bootloader?

As I have seen, an open bootloader middleware is offered for the STM32G4. An FDCAN implementation can be found here. Are there any plans to also offer a pure CAN implementation?

I am also interested in whether it is possible to program directly via CAN using the CubeProgrammer and the STLinkV3? In this case it would be conceivable for me to write a CAN implementation myself based on the open bootloader.

Best Ben!

This topic has been closed for replies.
Houda GHABRI
Houda GHABRIBest answer
ST Employee
Aug 11, 2021 3:33 PM UTC

Hi ben5en,

Yes, the programming via CAN is supported by CubeProgrammer and the STLinkV3 however the FDCAN is not supported .

Hope this helps you.

Houda

1 reply

Houda GHABRI
Houda GHABRIBest answer
ST Employee
Aug 11, 2021 3:33 PM UTC

Hi ben5en,

Yes, the programming via CAN is supported by CubeProgrammer and the STLinkV3 however the FDCAN is not supported .

Hope this helps you.

Houda