Skip to main content
ABasi.2
Senior
Feb 12, 2025 7:49 AM UTC
Solved

are printf, fprintf, scanf etc threadSafe in threadX?

HI

i have a question about printf. fprintf,scanf etc

i'm redirecting those functions to use a UART replacing the int _write(int file, char *ptr, int len)  and int _read(int file, char *ptr, int len) functions.

 

 

int _write(int file, char *ptr, int len)
{ 
 HAL_UART_Transmit(&huart2,(uint8_t*)ptr, len, 1000); 
 return len;
}

int _read(int file, char *ptr, int len)
{ 
 __HAL_UART_CLEAR_OREFLAG(&huart2);
 HAL_UART_Receive(&huart2,(uint8_t*)ptr, len,HAL_MAX_DELAY);
 HAL_UART_Transmit(&huart2,(uint8_t*)ptr,len, 1000); 
 return len;
}

 

 

 

now i'm using threadX and possibily call printf or the other function from multiple threads

is this approach already thread safe or i have to implement a mutex for the Uart?

If i have to use a mutex is that possible to get and put the mutex inside the _write or _read function or i have to get the mutex before call printf?

thank you

 

 

This topic has been closed for replies.
Saket_OmBest answer
ST Technical Moderator
Feb 12, 2025 10:12 AM UTC

Hello @ABasi.2 

To ensure thread safety, you need to use a mutex to protect the UART access. You can implement the mutex within the _write and _read functions, or you can acquire the mutex before calling printf or other related functions.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

3 replies

mbarg.1
Senior III
Feb 12, 2025 9:11 AM UTC

I feel confused - functons make operations on data, functions are non-atomic, therefore task can interrupt execution and pass control to other task that can make changes to data, when executon is resumed, data can be changed or corrupted ...

All data must be protected before executing non atomic functions !

Unless you are 100% sure that no other function will access the same data ...

Saket_OmBest answer
ST Technical Moderator
Feb 12, 2025 10:12 AM UTC

Hello @ABasi.2 

To ensure thread safety, you need to use a mutex to protect the UART access. You can implement the mutex within the _write and _read functions, or you can acquire the mutex before calling printf or other related functions.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
ABasi.2
ABasi.2Author
Senior
Feb 12, 2025 12:39 PM UTC

thank you!

i have modified my code like this :

int _write(int file, char *ptr, int len)
{ 
 if(tx_mutex_get(&consoleMutex,TX_WAIT_FOREVER) == TX_SUCCESS)
 {
 HAL_UART_Transmit(&huart2,(uint8_t*)ptr, len, 1000);
 tx_mutex_put(&consoleMutex);
 return len;
 }
 return 0; 
}

and it works fine

 

best reguards