Skip to main content
RAltm
Senior
May 3, 2026
Question

Arbitrary waveform by timer using DMA

Hello,

I want to generate an arbitrary waveform by a timer using DMA. The waveform is using different pulse widths and also varying periods in multiples of 25µs.

By reading AN4776 and HAL documentation I figured out it should be possible with HAL_TIM_DMABurst_MultiWriteStart() function. Unfortunately I don't get an output signal except after reset where a short pulse can be seen. I assume this pulse is due to port configuration during initialization. After that pulse, the signal stays high.

My setup (CubeMX):

  • Nucleo32-L432, core clock 80MHz
  • Used timer is Tim16
    • Prescaler is set to 399 => 80 MHz / 400 = 5µs resolution
    • ARR and CCR preload enabled
    • ARR and CCR set to 0 (initialized in source code)
    • DMA enabled
      • normal mode
      • memory to peripheral
      • Word / Word
      • increment address on memory
      • interrupt enabled

For a first run I want to use fixed pulse widths and varying periods, so all my code does is the following:

/* USER CODE BEGIN 2 */
htim16.Instance->ARR = 39;	//40 * 5µs = 200µs period
htim16.Instance->CCR1 = 4;	//5 * 5µs = 25µs pulse
HAL_TIM_DMABurst_MultiWriteStart(&htim16, TIM_DMABASE_ARR, TIM_DMA_UPDATE, (uint32_t *) Buffer, TIM_DMABURSTLENGTH_1TRANSFER, sizeof(Buffer) / sizeof(Buffer[0]));
HAL_TIM_PWM_Start(&htim16, TIM_CHANNEL_1);
/* USER CODE END 2 */

As far as I understood I need to initiate the first pulse by calling HAL_TIM_PWM_Start() and HAL_TIM_DMABurst_MultiWriteStart() setup the DMA to handle the subsequent transfers. 

When running that code, I get a single pulse of ~3.4µs at a period of 5.8µs, after that the output stays high. Since this is my first encounter with DMA I'm a bit lost. I don't get what I'm missing because other forum entries use basically the same approach as far as I can see.

Regards

14 replies

waclawek.jan
Super User
May 3, 2026

> ARR and CCR set to 0 (initialized in source code)

ARR = 0 means, that the timer is stopped. As you also set ARR preload, and there is no Update event which would transfer the new ARR to the "active" register and start the timer, so it remains stopped.

JW

RAltm
RAltmAuthor
Senior
May 3, 2026

Hello JW,

I tried both deactivating preload and using non-zero values for ARR/CCR directly in CubeMX. No change in behaviour. Any other ideas what might be the issue?

Regards

RAltm
RAltmAuthor
Senior
May 3, 2026

Update: seems that the silicon has a bug :( I used the Nucleo board reset button to restart and got the described behaviour. When doing a power reset it seems to (almost) work as expected.
I checked the errata sheet, but I couldn't find anything regarding the reset input only working partially...

Regards

waclawek.jan
Super User
May 4, 2026

I don't use Cube/CubeHAL, maybe there are some important details in that. And there may be also important details in the parts of your code we don't see (you could post a minimal but complete working example exhibiting the problem).

What is "(almost) work as expected"?

JW

Gyessine
ST Technical Moderator
May 4, 2026

Hello @RAltm 
Honestly, it will be helpfull if you provide more details about your application or share you main.c and msp.c files
but from global view, I think you should use circular mode not normal mode in your case
However, I attached a project that uses TIM16 with DMA to change content of ARR with different values as you wanted (3 values in this example 100,150,175)
You can base yourself on it, if it aligns with your demand 

Gyessine_0-1777903969440.png

BR
Gyessine
 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
RAltm
RAltmAuthor
Senior
May 4, 2026

@waclawek.jan wrote:

I don't use Cube/CubeHAL, maybe there are some important details in that. And there may be also important details in the parts of your code we don't see (you could post a minimal but complete working example exhibiting the problem).

What is "(almost) work as expected"?


I'll provide a MWE as soon as possible. However, first I want to check that reset behaviour. I expect the same behaviour when pressing the reset button or doing a power reset. Only on the latter I see the output pulses. I'll also provide screenshots from the logic analyzer for the two cases. I'll also check if I have a free Nucleo board with a different MCU type to compare the behaviour.

"Almost works as expected" means that I can see the expected output pulses (when doing a power reset), but the output goes high and stays high after the last pulse. I expected the output to stay low after the last pulse. I don't know if I have to disable DMA and/or the timer after the DMA signals the end of the transfer.


@Gyessine wrote:

Honestly, it will be helpfull if you provide more details about your application or share you main.c and msp.c files
but from global view, I think you should use circular mode not normal mode in your case
However, I attached a project that uses TIM16 with DMA to change content of ARR with different values as you wanted (3 values in this example 100,150,175)
You can base yourself on it, if it aligns with your demand  


Hello Gyessine, thank you for the project, I'll compare it to my implementation. As mentioned, I'll provide a MWE of my implementation as soon as possible.

However, I indeed want to use non-circular mode. I want to output a varying number of pulses with varying period and pulse duration. Between the pulse trains, the output should stay low and the next pulse train must not start before the period of the last pulse of the previous train has expired. As mentioned, I don't know if I have to disable DMA and/or the timer after the DMA signals the end of the transfer. I'd be glad if you can give me some hints.

Regards

waclawek.jan
Super User
May 4, 2026

> I expect the same behaviour when pressing the reset button or doing a power reset.

There are few things which behave differently upon power-on reset and NRST-reset. One of them is the PEMPTY bit behaviour, which is set if the FLASH is empty during reset (which may happen during programming after erase, depending on how exactly the programmer/debugger behaves), impacts the mapping at address 0, and is not reset by NRST, only by a power-on reset. The symptom involves the system-ROM (bootloader) being mapped at address 0, and usually interrupts then end up in the 0x1fffxxxx area. I guess there may be other mechanisms for different NRST/power-on behaviour. This is a recurring theme here, but rarely the user comes to a definitive conclusion.

How the pulse train ends depends on the PWM mode you are using, and the exact way how you end the pulse train and/or what do you exactly do with the output after the pulse train finishes. One way to tackle this is to set the last CCRx item to be 0 or ARR+1; those values should ensure the output to be a steady value of either polarity.

JW

RAltm
RAltmAuthor
Senior
May 4, 2026

@waclawek.jan wrote:

> I expect the same behaviour when pressing the reset button or doing a power reset.

There are few things which behave differently upon power-on reset and NRST-reset. One of them is the PEMPTY bit behaviour, which is set if the FLASH is empty during reset (which may happen during programming after erase, depending on how exactly the programmer/debugger behaves), impacts the mapping at address 0, and is not reset by NRST, only by a power-on reset. The symptom involves the system-ROM (bootloader) being mapped at address 0, and usually interrupts then end up in the 0x1fffxxxx area. I guess there may be other mechanisms for different NRST/power-on behaviour. This is a recurring theme here, but rarely the user comes to a definitive conclusion.


Interesting, thank you for pointing me to that. I checked the reference manual about the PEMPTY bit. If this bit is the issue, I'll try to modify it and enforce a software reset. From the description it might be the issue - I played with the reset settings in CubeIDE and interestingly it changed the behaviour after downloading the image (not debugging, only download). I've to verify it, but it looked like the program runs okay after download, then the timer output flipped after several milliseconds. Pressing the reset button resulted in the initial behaviour (no output). But as I said, I've to verify.

 

 


@waclawek.jan wrote:

How the pulse train ends depends on the PWM mode you are using, and the exact way how you end the pulse train and/or what do you exactly do with the output after the pulse train finishes. One way to tackle this is to set the last CCRx item to be 0 or ARR+1; those values should ensure the output to be a steady value of either polarity.


I will try that, good point, thank you. Currently I'm using the period elapsed callback from DMA and disable the timer, but this shortens the last pulse. Your approach is promising because it would enable to keep the full period of the last visible pulse. If I remember correctly I initially tried one additional ARR item with value 0 to stop the timer, but that resulted in the output going high.

Regards

Gyessine
ST Technical Moderator
May 5, 2026

Hello @RAltm 
>However, I indeed want to use non-circular mode. I want to output a varying number of pulses with varying period and pulse duration. Between the pulse trains, the output should stay low and the next pulse train must not start before the period of the last pulse of the previous train has expired

This task can be challenging if you want to achieve clean results.
Using DMA in normal mode typically generates a continuous PWM signal, with the last value in the pulse train remaining at the ARR. To generate a second pulse train, you must stop the PWM and restart it.

You can apply the following modifications to the previous project to address this use case:
The configuration creates a pulse train with values of 100, 150, and 175, then stops (with the PWM signal held low) until you start the timer with a new pulse train.

/* USER CODE BEGIN PD */
#define ARR_WAVEFORM_LEN (sizeof(arr_waveform) / sizeof(arr_waveform[0]))

/* USER CODE END PD */
/* USER CODE BEGIN PV */
volatile uint32_t dma_cndtr_start = 0;
volatile uint32_t dma_cndtr_now = 0;
volatile uint8_t dma_done = 0;
/* USER CODE END PV */
/* USER CODE BEGIN PFP */
void MyDMADoneCallback(DMA_HandleTypeDef *hdma);

/* USER CODE END PFP */
/* USER CODE BEGIN 2 */
 uint16_t arr_waveform[] = {100, 150, 175,175};

 __HAL_TIM_SET_AUTORELOAD(&htim16, arr_waveform[0]);
 __HAL_TIM_SET_COMPARE(&htim16, TIM_CHANNEL_1, 50);

 HAL_DMA_RegisterCallback(htim16.hdma[TIM_DMA_ID_CC1],
 HAL_DMA_XFER_CPLT_CB_ID,
 MyDMADoneCallback);

 if (HAL_DMA_Start_IT(htim16.hdma[TIM_DMA_ID_CC1],
 (uint32_t)(arr_waveform),
 (uint32_t)&TIM16->ARR,
 ARR_WAVEFORM_LEN) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_TIM_ENABLE_DMA(&htim16, TIM_DMA_CC1);

 if (HAL_TIM_PWM_Start(&htim16, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }

 if (HAL_TIM_Base_Start_IT(&htim16) != HAL_OK)
 {
 Error_Handler();
 }

 /* USER CODE END 2 */



/* USER CODE BEGIN 4 */

void MyDMADoneCallback(DMA_HandleTypeDef *hdma)
{
 dma_done = 1;
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
 if (htim->Instance == TIM16 && dma_done)
 {
 dma_done = 0;
 __HAL_TIM_DISABLE_DMA(&htim16, TIM_DMA_CC1);
 HAL_TIM_Base_Stop(&htim16);
 HAL_TIM_PWM_Stop(&htim16, TIM_CHANNEL_1);
 }
}
/* USER CODE END 4 */

verify that dma configuration in msp.c is like this :

void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base)
{
 if(htim_base->Instance==TIM16)
 {
 /* USER CODE BEGIN TIM16_MspInit 0 */

 /* USER CODE END TIM16_MspInit 0 */
 /* Peripheral clock enable */
 __HAL_RCC_TIM16_CLK_ENABLE();

 /* TIM16 DMA Init */
 /* TIM16_CH1_UP Init */
 hdma_tim16_ch1_up.Instance = DMA1_Channel3;
 hdma_tim16_ch1_up.Init.Request = DMA_REQUEST_4;
 hdma_tim16_ch1_up.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_tim16_ch1_up.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_tim16_ch1_up.Init.MemInc = DMA_MINC_ENABLE;
 hdma_tim16_ch1_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
 hdma_tim16_ch1_up.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
 hdma_tim16_ch1_up.Init.Mode = DMA_NORMAL;
 hdma_tim16_ch1_up.Init.Priority = DMA_PRIORITY_LOW;
 if (HAL_DMA_Init(&hdma_tim16_ch1_up) != HAL_OK)
 {
 Error_Handler();
 }

 /* Several peripheral DMA handle pointers point to the same DMA handle.
 Be aware that there is only one channel to perform all the requested DMAs. */
 __HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_CC1],hdma_tim16_ch1_up);
 __HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_UPDATE],hdma_tim16_ch1_up);

 /* TIM16 interrupt Init */
 HAL_NVIC_SetPriority(TIM1_UP_TIM16_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(TIM1_UP_TIM16_IRQn);
 /* USER CODE BEGIN TIM16_MspInit 1 */

 /* USER CODE END TIM16_MspInit 1 */

 }

}

You should get a result like this :

Gyessine_0-1777994760837.png

BR
Gyessine



In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
RAltm
RAltmAuthor
Senior
May 5, 2026

@waclawek.jan 
Update: I switched to a L082 device. Here, the reset behaviour after downloading is as expected. No need to do a power-reset as far as I can see by now. So, figuring out what's going on on the L432 device needs investigation.

Indeed the PEMPTY flag was set after download, but not always. So, the behaviour when doing a software reset if PEMPTY flag is set and cleared was more reliable, but it seems there's still other magic happening. Thanks again for pointing me to that detail. The code snippet I used:

if(0 != __HAL_FLASH_GET_FLAG(FLASH_FLAG_PEMPTY)) {
	SET_BIT(FLASH->SR, FLASH_FLAG_PEMPTY);	//bit is toggled when set
	NVIC_SystemReset();
}

@Gyessine 
Thank you for that detailed description and code snippets. Some questions:

  • The variables dma_cndtr_start​ and dma_cndtr_now are defined, but not used. So I assume they're not relevant, right?
  • The difference to using HAL_TIM_DMABurst_MultiWriteStart() function is that
    • the timer uses both IRQ and DMA setup
    • the timer interrupt fires on each period
    • only when the DMA is done the timer interrupt stops DMA and the timer itself
      Is the above true? If yes, it's done this way because it's easier to manage than by HAL_TIM_DMABurst_MultiWriteStart() function, right?

Regards

Gyessine
ST Technical Moderator
May 6, 2026

Hello @RAltm 

The variables defined in the private variables section are irrelevant. They were included for testing purposes and should have been removed. I apologize for the confusion.

I think your task is achievable using HAL_TIM_DMABurst_MultiWriteStart. However, this is not its main purpose. The main purpose of HAL_TIM_DMABurst_MultiWriteStart is to allow DMA to update a block of timer registers, not just one register. That is why I did not use it, but you can try it. It is a matter of preference, not correctness.

> I switched to an STM32L082 device. Here, the reset behavior after downloading is as expected. There is no need to perform a power reset as far as I can see. Investigating the reset behavior on the STM32L432 device is still required.

About this reported issue: it is different from the question you started this thread with. For moderation purposes, I suggest you post your new issue in a separate thread and close this thread if it is resolved or if you are now interested in your new question.
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
RAltm
RAltmAuthor
Senior
May 6, 2026

Hello Gyessine,

as I wrote here I also want to change the pulse width, I just started with one register to keep it as easy as possible. So I'll try to adapt your approach to HAL_TIM_DMABurst_MultiWriteStart. Your examples gave a good insight, thank you for that.

Regarding the reported issue: basically it wasn't a software issue, but the device behaviour which caused the issue. So, I agree that different issues shouldn't be mixed, although we did it by focusing on DMA handling, not the reset issue.
Question: shall I modify the topic title to better reflect that it's been related to device behaviour or should I really create a new topic especially for the reset behaviour?

If we agree that the real issue is the reset behaviour of the L432, there's no solution yet. If we decide that the goal of having a working DMA transfer has been reached, I can mark one of the postings as solution (currently I don't care if it works on L432 or L082) and I create a new topic about the reset stuff. I any case I think it would need pointing someone from ST to it.

Regards

waclawek.jan
Super User
May 7, 2026

> reset behaviour of the L432, there's no solution yet

Before enabling any interrupt (i.e. in startup or very beginning of main()):

- set SCB_VTOR to 0x0800'0000 - there may be some Cube-specific way to do that, as I've said, I don't use Cube

- set SYSCFG_MEMRMP.MEM_MODE to 0b000 to explicitly map main FLASH to 0x0000'0000

JW

Gyessine
ST Technical Moderator
May 7, 2026

Hello @RAltm 
Honestly, I recommend that you post the reset issue in a new thread. Explain the test scenario, the expected behavior, and the observed behavior in detail.
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.