Skip to main content
DK.7
Associate III
Jul 17, 2022 10:36 AM UTC
Question

Application that use FreeRTOS doesn't start properly from external QSPI chip.

Could someone tell me, what i do wrong?

I made an external bootloader on QuadSPI chip and it works well with applications that do not use a FreeRTOS!

But, I need to make the application that use FreeRTOS and it is don't work properly!

The steps that I have done:

1. I added in to code of "External Bootloader" line

__set_CONTROL(0);

2. In my linker script of "My_FeeRTOS_application" I changed a line according size of my QuadSPI chip

FLASH (rx)  : ORIGIN = 0x90000000, LENGTH = 8M

3. In file "system_stm32h7xx.c" I added in SystemInit line

SCB->VTOR = QSPI_BASE;

Maybe I need to add something else?

This topic has been closed for replies.