Skip to main content
Associate II
Feb 13, 2026 2:20 AM UTC
Question

An exception occurred after using HAL_UART_Transmit_DMA with HAL_UART_AbortReceive.

Chip model: STM32H723VGTx
Both the RX and TX buffers are allocated in the D2 domain.

1.CubMx settings are correct.
2.HAL_UART_Transmit_DMA runs normally on the first run.

However, after running HAL_UART_AbortReceive, HAL_UART_Transmit_DMA fails.

Tracing the HAL_UART_Transmit_DMA function:
The huart->gState value is always 0x33.

7 replies

ST Technical Moderator
Feb 13, 2026 9:39 AM UTC

Hello @YutinhLin 

Why you are calling HAL_UART_AbortReceive() after a transmit operation?

If your intention is to abort an ongoing transmission, you should use HAL_UART_AbortTransmit() instead.

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
YutinhLinAuthor
Associate II
Feb 13, 2026 9:46 AM UTC

I use `INFO.RX.count=CO_UART_BUF_LENGTH-(__HAL_DMA_GET_COUNTER(CO_INFO.channel->hdmarx));` to calculate the data index,
and I need to reset the index to 0 each time.

So I tried using `HAL_UART_AbortTransmit()`, but it didn't work.
Then I tried using `HAL_UART_AbortReceive()`, and it worked.

ST Technical Moderator
Feb 13, 2026 10:20 AM UTC

Hello @YutinhLin 

You should investigate why HAL_UART_AbortTransmit() is not working. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
TDK
Feb 16, 2026 5:53 AM UTC

Duplicate:

STM32H723VGTx DMA TX reboot use fail - STMicroelectronics Community

 

If you're using HAL functions, you need to abide by their rules. Calling HAL_UART_AbortReceive to abort a transmit still makes no sense.

"If you feel a post has answered your question, please click ""Accept as Solution""."
YutinhLinAuthor
Associate II
Feb 23, 2026 1:59 AM UTC

This is a very strange phenomenon, but you don't see it as a problem.

Okay, I tried using HAL_UART_AbortTransmit() to stop the DMA transfer, but the same HAL_UART_Transmit_DMA() didn't work.

The error code for huart->gState changes to 0x32.

This is my call enable and disable function :
void CO_DMA_CRL(FunctionalState state)
{
if(state==DISABLE)
{
if(HAL_OK==HAL_UART_AbortReceive(CO_INFO.channel))
CO_INFO.dma_status=DISABLE;
if(HAL_OK==HAL_UART_AbortTransmit(CO_INFO.channel))
CO_INFO.dma_status=DISABLE;
}
else
{
CO_INFO.RX.data = (uint8_t *)co_dma_rx_data;
if(HAL_OK==HAL_UARTEx_ReceiveToIdle_DMA(CO_INFO.channel,(uint8_t*)CO_INFO.RX.data,CO_UART_BUF_LENGTH))
CO_INFO.dma_status=ENABLE;
}
}

Then I tried adding reinitialization:
MX_DMA_Init();
MX_BDMA_Init();
The error code for huart->gState became 0x33.

The HAL library was originally intended to be easy for developers to use.
Furthermore, why do the TX settings of DMA interact with the RX settings?

My initial use case was that I needed to reset the receive index to 0 each time.
As I mentioned in another post,When TX calls DMA, does the state not automatically return to IDLE after data transfer is complete?

The problem is that when using the HAL library, DMA TX fails to function properly after using HAL_UART_AbortReceive(), and re-executing MX_DMA_Init() and MX_BDMA_Init() also fails.
Do you mean I should abandon the HAL library and study the specs myself to achieve my desired development goals?

TDK
Feb 24, 2026 3:35 AM UTC

If you provide the actual code being used that replicates the problem, I will check it out.

Break it down into a few different HAL_* calls that illustrates the issue, like I did in your other thread with code that works. Not just function names, but actual code.

"If you feel a post has answered your question, please click ""Accept as Solution""."