Skip to main content
Associate III
Dec 20, 2024 12:49 AM UTC
Solved

Alternative ethernet driver for the NUCLEO-H7S3L8

I am trying to prototype ethernet on the NUCLEO-H7S3L8 eval board. When enabling ethernet through CubeMx using the same configuration I've used on the NUCLEO-H563ZI, the ethernet driver fails initialization.

 

Is there an alternative Ethernet driver that is recommended or a better eval board I should use?

This topic has been closed for replies.
ASEHSTBest answer
ST Employee
Dec 23, 2024 8:50 AM UTC

Hello @potatobandit 

 

This tutorial may be helpful: How to create a project for STM32H7 with Ethernet ... - STMicroelectronics Community, which provides Ethernet example for STM32H7. The same steps should be applicable to the STM32H7S3L8.

Additionally, various LwIP examples can be found here: STM32CubeH7RS - NUCLEO-H7S3L8 Applications, which might be helpful as a starting point.

 

With Regards,

 

"If your question is answered, please close this topic by clicking ""Accept as Solution""."

2 replies

Pavel A.
Dec 20, 2024 2:04 AM UTC

This board has LwIP examples. Please start from one of the examples and make it work on your board before creating a new project from scratch (.ioc)

 

ASEHSTBest answer
ST Employee
Dec 23, 2024 8:50 AM UTC

Hello @potatobandit 

 

This tutorial may be helpful: How to create a project for STM32H7 with Ethernet ... - STMicroelectronics Community, which provides Ethernet example for STM32H7. The same steps should be applicable to the STM32H7S3L8.

Additionally, various LwIP examples can be found here: STM32CubeH7RS - NUCLEO-H7S3L8 Applications, which might be helpful as a starting point.

 

With Regards,

 

"If your question is answered, please close this topic by clicking ""Accept as Solution""."