Skip to main content
VKUMA.12
Associate III
Aug 21, 2019 10:27 AM UTC
Solved

After upgrading firmware in stm32f407vgt through pendrive fatfs of upgraded code is not working, controller hangs on f_mount, please help...............

..

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 21, 2019 12:34 PM UTC

Instrument code so you know what's going on.

Make sure interrupts are functioning, and vector table address is set correctly.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

7 replies

Ozone
Principal
Aug 21, 2019 10:33 AM UTC

We are supposed to speak magic workd into crystal balls ? A bit more information would be helpful.

Have you validated the updat eprocess itself and the new firmware version (update) independently ?

VKUMA.12
VKUMA.12Author
Associate III
Aug 21, 2019 11:39 AM UTC

thanks for reply......

am upgrading firmware in microcontroller using a usb pendrive, any other program other than usb works fine.

there are two program running on the controller, first is firmware upgrade program and another is the program we want to upload in microcontroller using usb

pendrive. From reference manual AN3990

Ozone
Principal
Aug 21, 2019 12:27 PM UTC

Not easy to comrehend what you mean.

>... first is firmware upgrade program ...

A bootloader, to check for updates, and perform them if necessary ?

>... and another is the program we want to upload in microcontroller ...

The application supposed to run normally ?

Have you tried to debug your code ?

Where does it get stuck, or faults ?

> ... hangs on f_mount ...

Did you check why f_mount fails, down to the peripheral driver level ?