Skip to main content
Associate II
Apr 7, 2025 7:41 AM UTC
Question

After STOP2 Mode Wake-Up

STM32L496VET6 – EXTI Not Working After STOP2 Mode Wake-Up

1. Part Number

  • STM32L496VET6, LQFP100

  • Custom-designed hardware (not a development board)


2. Environment

  • IDE: STM32CubeIDE v1.15.0

  • STM32CubeMX: v6.11.0

  • HAL Driver Package: STM32CubeL4 v1.18.0

  • Toolchain: GCC Embedded

  • Debugger: ST-LINK V3

  • Host OS: Windows 11


3. Schematics

  • Pin PE0 is connected to a push-button with an external 10kΩ pull-up resistor to VDD.

  • PE0 is configured as a falling-edge EXTI input (GPIO_EXTI0).

  • Schematic is available if needed.


4. Details (Symptoms)

  • EXTI on PE0 (EXTI0) works correctly before entering STOP2 mode.

  • After entering STOP2 using HAL_PWREx_EnterSTOP2Mode(), the device does not wake up when the PE0 button is pressed.

  • No interrupt is triggered, and the MCU remains in low power mode.


5. Expected Behavior

  • A falling edge on PE0 should trigger an interrupt and wake the MCU from STOP2 mode.

  • The MCU should resume operation, restore clocks, and continue running code.


6. How to Reproduce

  1. Configure PE0 as GPIO_EXTI0 in CubeMX (falling edge, no pull).

  2. In code:

    • Enable SYSCFG and GPIOE clocks.

    • Set EXTI source with:

      c
      CopyEdit
      LL_SYSCFG_SetEXTISource(LL_SYSCFG_EXTI_PORTE, LL_SYSCFG_EXTI_LINE0);
    • Configure PE0 as falling-edge interrupt.

    • Enable EXTI0_IRQn interrupt.

    • Suspend SysTick and enter STOP2:

      c
      CopyEdit
      HAL_SuspendTick(); HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
    • After wake-up, call SystemClock_Config() and reinitialize GPIO and EXTI.

  3. Press the push-button connected to PE0 while in STOP2.


7. Occurrence

  • The issue is consistently reproducible.

  • The system wakes up and triggers EXTI correctly when not using STOP2.

  • The issue only occurs after entering STOP2.


8. Sanity Checks Performed

  • Verified EXTI0 interrupt handler is implemented correctly and functional.

  • Verified PE0 EXTI works perfectly before STOP2.

  • Clocks are properly restored after STOP2 using SystemClock_Config().

  • Re-initialized EXTI and GPIO after wake-up.

  • Ensured PE0 is not used by debug interface (no conflict with TRACECLK).

  • Tried using LL drivers directly for EXTI instead of HAL.

  • Added pull-up to PE0 for stable signal level.

  • Tested wake-up from PA0 using HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1), which works correctly.

void PowerDownUp(uint8_t Powermode)
{
//	HAL_SuspendTick();
//
//	PowerDown_GPIO_Deinit();
////		GPIO_InitTypeDef GPIO_InitStruct = {0};
////
//		__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF2);
////
////
////
////		HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2_HIGH);
////
//		HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
//
//
//
////================ Init Modules===================================================//
//
////	SystemReInit();
//		SystemClock_Config();
//
//		HAL_GPIO_WritePin(LED_RED_GPIO_Port, LED_RED_Pin, SET);
//		HAL_ResumeTick();

//	__HAL_RCC_SYSCFG_CLK_ENABLE();

 HAL_SuspendTick();


 __HAL_RCC_SYSCFG_CLK_ENABLE();

 // 2. Remap EXTI0 to PE0
 LL_SYSCFG_SetEXTISource(LL_SYSCFG_EXTI_PORTE, LL_SYSCFG_EXTI_LINE0);

 // 3. Re-init GPIO pin PE0
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_PULLUP; // Optional: adds stability if PE0 is floating
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
// __HAL_RCC_LSECSS_EXTI_ENABLE_IT();
 HAL_GPIO_WritePin(LED_GREEN_GPIO_Port, LED_GREEN_Pin, RESET);
// HAL_RCC_LSICmd(ENABLE);
 NVIC_EnableIRQ(EXTI0_IRQn);
 HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);

 // Restore clocks
 SystemClock_Config();

 // Re-initialize GPIOs including EXTI pin
 SystemReInit(); // or reconfigure the EXTI pin here manually

 // Debug
 HAL_ResumeTick();
}
This topic has been closed for replies.

1 reply

ST Technical Moderator
Apr 10, 2025 10:53 AM UTC

Hello @Chintu 

Did you check this example please?

If you still have the issue, please share your project if possible.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om