Skip to main content
Associate
Jul 8, 2025 6:58 PM UTC
Question

ADDRERRF bit getting set on PKA init

Hello,

I am trying to use the PKA module on a STM32U5 controller. I have configured the clock at 160Mhz and also initialized the Ring. However, when I try to initialize the PKA, it runs into ADDRERRF = 1, I was expecting ofcourse INITOK to be 1. Does anyone have Idea what am I missing here or what might be causing the ADDRERRF?

 

Thanks,

Abhi

This topic has been closed for replies.

4 replies

Associate
Jul 8, 2025 7:39 PM UTC

Trying to clarify to avoid misunderstanding. I meant both the bits ADDRERRF and INITOK are set to 1 after I call the init function. I see in the debugger that the RNG is running.

ST Technical Moderator
Jul 10, 2025 3:00 PM UTC

Hello @abhisheksirsikar 

Are you using the HAL library? 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Associate
Jul 10, 2025 8:10 PM UTC

yes. I just ignored the error bit and everything works as expected. But I couldn’t figure out why the error bit is getting set

Billy OWEN
ST Employee
Jul 17, 2025 7:40 PM UTC

Hi @abhisheksirsikar 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy