Skip to main content
coso2
Associate II
Jan 23, 2025 11:11 PM UTC
Question

Adding BSD sockets to netxDuo for LLDP

Hi,

I was able to run a demo project on a STM32H573 dev board. I am using ThreadX and NetxDuo, with mqtt addon.

I was able to connect to the mqtt broker and send/receive messages.

I want also to be able to use the bsd sockets to send packets on layer 2. As far as I have understood, for sending and receiving layer 2 packets I need to use bsd sockets.

I followed the doc from github, added the files .h and .c 
I had to add the line

#define TX_THREAD_USER_EXTENSION int bsd_errno


in the user code part of "tx_user.h", so it can survive a code generation.

Then I enabled 
NX_ENABLE_EXTENDED_NOTIFY_SUPPORT
and

NX_ENABLE_IP_RAW_PACKET_FILTER

Then I got into a problem: the redefinitions of structs and function names, so I added

#define NX_BSD_ENABLE_NATIVE_API

in the user code part of "nx_user.h"
I want to have raw support, so I also added

#define NX_BSD_RAW_SUPPORT

in the user code part of "nx_user.h"

Now I get an error when I compile:
"nxd_bsd.c:474: undefined reference to `_nx_driver_hardware_packet_received_callback' "

Am I missing something or I am doing it wrong? 
Thanks in advance tor any help

This topic has been closed for replies.

4 replies

coso2
coso2Author
Associate II
Jan 24, 2025 11:02 PM UTC

Ok, I got something in working condition.. kinda. I can init and create a raw socket.

Now, if I call the function "nx_bsd_send", the compiler is complaining abount this:

../NetXDuo/App/nxd_bsd.c:13327: undefined reference to `_nx_driver_hardware_packet_send'

that line is in the function

static INT _nx_bsd_hardware_internal_sendto(NX_BSD_SOCKET *bsd_socket_ptr, CHAR *msg, INT msgLength, INT flags, struct nx_bsd_sockaddr* destAddr, INT destAddrLen)

If I go to that line and press F3, I go to the declaration in nxd_bsd.h file:

extern UINT _nx_driver_hardware_packet_send(NX_PACKET *packet_ptr);

If I press again F3, I go straight to the implementation in the file "nx_stm32_eth_driver.c".

How is it possible for the ide to find the function, but when I compile I get undefined reference?

Thanks for any hint or advise

ST Employee
Feb 17, 2025 4:19 PM UTC

Hello @coso2 ,

This is clearly an include path problem it's normal that IDE recognizes the function and the compiler doesn't as it needs to have a path to the file where the function was declared.
Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
coso2
coso2Author
Associate II
Feb 18, 2025 9:53 PM UTC

The function "_nx_driver_hardware_packet_send" in "nx_stm32_eth_driver.c" is static

 

 

static VOID _nx_driver_packet_send(NX_IP_DRIVER *driver_req_ptr)

 

 

And every time I generate the code, I have to manually remove the "static" keyword

Associate III
Feb 24, 2025 6:27 PM UTC

I am having the exact same issue. 

The function "_nx_driver_hardware_packet_send" in "nx_stm32_eth_driver.c" is static and the "nxd_bsd.h" file has that function externed. Therefore, the only way for this addon to work is to go and edit the file every time. 

NXD_BSD also externs `_nx_driver_hardware_packet_received_callback` when we enable NX_BSD_RAW_SUPPORT. This function doesn't seem to exist at all in the ethernet driver. 

Does ST have any instructions for integrating the NXD_BSD addon into a H7 project using the NX_BSD_RAW_SUPPORT defined? This flag seems to be required if you want to support multicasting.