Skip to main content
Associate
Jul 7, 2025 3:03 PM UTC
Solved

ADC1/2 not working over DMA on NUCLEO-H7A3ZI-Q (+Azure RTOS)

Dear community,

I have a NUCLEO-H7A3ZI-Q board with CAN, USART, USB Device and 4 analog inputs. My application is structured using the Azure RTOS, but for ADC testing purposes I am not calling MX_ThreadX_Init() anymore. With the AZRTOS initiated is the same ADC behavior.

The example at https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/NUCLEO-H7A3ZI-Q/Examples/ADC/ADC_DMA_Transfer works, but they only use 1 channel. The board and at least ADC_Channel11 works.

I attached my IOC file, but basically I am using ADC2 (also tried with ADC1) in continuous conversion, DMA circular mode.

I also attached the main.c file. The gist of it:

ALIGN_32BYTES (static uint16_t ADC_VAL[4]);
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
if (hadc == &hadc2) {
ADCfinished = 1; // Set the flag to indicate conversion is complete
}
}

// in main()...
if (HAL_ADC_Start_DMA(&hadc2, (uint32_t *) ADC_VAL, 4) != HAL_OK)
{
Error_Handler();
}

while (1)
{
if (ADCfinished) {
// print the ADC_VAL array
printf("ADC Values: %u, %u, %u, %u\n",
(unsigned int) ADC_VAL[0],
(unsigned int) ADC_VAL[1],
(unsigned int) ADC_VAL[2],
(unsigned int) ADC_VAL[3]);
ADCfinished = 0; // Reset the flag
} // end if
HAL_Delay(250); // Delay for 1 second to allow ADC to stabilize
} // end while

The defined interrupt handler never gets invoked. (If I turn off DMA and use HAL_ADC_Start_IT(), the interrupt is getting called)

By tracing and using some AI magic, I found out that the register DMA1->S0CR->EN is 0 (not enabled). In the HAL_ADC_Start_DMA() function, the call to HAL_DMA_Start_IT() sets this register. However, the very next call (LL_ADC_REG_StartConversion(hadc->Instance);) disables the register.

Can anyone please take a look and tell me what am I missing? What combination of settings are disabling the DMA? Any help is greatly appreciated!

 

Best regards,

Cristian.

 

This topic has been closed for replies.
tuduceBest answer
Associate
Jul 7, 2025 8:05 PM UTC

I found the solution using https://community.st.com/t5/stm32-mcus/dma-is-not-working-on-stm32h7-devices/ta-p/49498

The buffer (ADC_VAL[]) was in the DTCMRAM, where the DMA1 can't access it. When moving the buffer to RAM (starting at 0x24000000) DMA works as expected.

 

Cheers,
Cristian

4 replies

Karl Yamashita
Super User
Jul 7, 2025 7:46 PM UTC

You main.c is missing code for MX_ADC2_Init()

I can't seem to import your IOC file? It imports only as a Project, but no IOC file to view any settings.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
tuduceAuthor
Associate
Jul 7, 2025 7:59 PM UTC

Hi,

thanks for looking into this!

The call to

MX_ADC2_Init();

is after

MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();

 I don't know what to say about the IOC file. If I download the attached IOC and look at it with a text editor, it looks like an IOC-file.

 

Cheers,

Cristian.

Karl Yamashita
Super User
Jul 7, 2025 8:29 PM UTC

@tuduce wrote:

Hi,

thanks for looking into this!

The call to

MX_ADC2_Init();

is after

MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();

 I don't know what to say about the IOC file. If I download the attached IOC and look at it with a text editor, it looks like an IOC-file.

 

Cheers,

Cristian.


For some reason, my STM32CubeIDE 1.18.1 which I've been using for weeks, started having issues today, even when creating new projects. An IOC file is never created. I just now upgraded to 1.19.0 and it opens the IOC file correctly.

But that's good that you've found a fix.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
tuduceAuthorBest answer
Associate
Jul 7, 2025 8:05 PM UTC

I found the solution using https://community.st.com/t5/stm32-mcus/dma-is-not-working-on-stm32h7-devices/ta-p/49498

The buffer (ADC_VAL[]) was in the DTCMRAM, where the DMA1 can't access it. When moving the buffer to RAM (starting at 0x24000000) DMA works as expected.

 

Cheers,
Cristian