Skip to main content
Associate III
Nov 22, 2024 6:57 AM UTC
Question

ADC generates power consumption after stm32L4 enters stop mode

I use STM32L431 to enter STOP1 mode, the original power consumption is 53uA. Before entering stop mode, I call HAL_ADC_DeInit(&hadc1) to disable ADC, and call MX_ADC1_Init() to re-enable ADC after exiting STOP1 mode. The measured power consumption is 66uA, which is about 10uA more. Why? If I do not call MX_ADC1_Init() after exiting STOP1 mode, the power consumption is still 53uA. Is it because ADC will generate power consumption?

Below is my code to enter and exit STOP1:

void EnterStop2ModeRTC(void)
{
 HAL_RCCEx_WakeUpStopCLKConfig(RCC_STOP_WAKEUPCLOCK_MSI);
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
 __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);
 __HAL_RTC_WAKEUPTIMER_EXTI_CLEAR_FLAG();
 __HAL_RTC_TIMESTAMP_CLEAR_FLAG(&hrtc, RTC_FLAG_TSF);
 __HAL_RTC_TAMPER_TIMESTAMP_EXTI_CLEAR_FLAG();
 HAL_ADC_DeInit(&hadc1);
 HAL_SuspendTick();
 // __HAL_RCC_DMA1_CLK_DISABLE();
 cpuStopFlg = true;
 SCB->SCR |= SCB_SCR_SLEEPONEXIT_Msk;
 __HAL_RCC_PWR_CLK_ENABLE();
 HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI); 
}

void ExitStop2ModeRTC(void)
{
 SystemClock_Config();
 HAL_ResumeTick();
 MX_ADC1_Init();
 cpuStopFlg = false;
}

 

This topic has been closed for replies.

5 replies

ST Employee
Nov 25, 2024 10:00 AM UTC

Hello @AlfRomeo,

HAL_ADC_MspInit() calls typically bus clock activation: __HAL_RCC_ADC_CLK_ENABLE().
Can you check whether you have implemented HAL_ADC_MspDeInit() in your application ?
If yes, does it contain bus clock deactivation: __HAL_RCC_ADC_CLK_DISABLE(); __HAL_RCC_ADC_FORCE_RESET(); __HAL_RCC_ADC_RELEASE_RESET() ?

I hope my answer has helped you. When your question is answered, please select this topic as solution that answered you, it will help others find that answer faster.

Thanks for your contribution.

Dor_RH

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Dor_RH
AlfRomeoAuthor
Associate III
Nov 26, 2024 12:05 AM UTC

I did not use the HAL_ADC_MspInit() function, I directly used HAL_ADC_DeInit (&hadc1);

ST Employee
Nov 26, 2024 10:06 AM UTC

Hello @AlfRomeo,

Could you try to Implement the HAL_ADC_MspDeInit() function: it frees the hardware resources used:

  • Disable the Peripheral's clock
  • Revert GPIO to their default state

I hope my answer has helped you. When your question is answered, please select this topic as solution that answered you, it will help others find that answer faster.

Thanks for your contribution.

Dor_RH

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Dor_RH