Skip to main content
dhiry2k
Associate II
December 11, 2012
Question

Activating USB core clock disables the Ethernet link

  • December 11, 2012
  • 2 replies
  • 653 views
Posted on December 11, 2012 at 12:14

Hi,

I am working on USB and Ethernet integration with USART. My ethernet Application is running perfectly and i am inserting code for USB into it. I noticed when i enable USB core clock, The ethernet link disconnects and my LCD shows '' Network Cable is unplugged'' I dont know why this is happening ?

Anyone had the same issue?  I am using STM32F207 USB and Lwip Libraries. with STM3220G-EVAL Board.

Thanks,

Dheeraj

#connectivity-usb #ethernet-interface #stm32
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
December 11, 2012
Posted on December 11, 2012 at 17:16

I've not heard of an issue.

You should perhaps look over the schematic and pin utilization to see if there is an interfacing conflict. Consider also if the board implements a MII or RMII interface, and where it derives it's clock.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
dhiry2k
dhiry2kAuthor
Associate II
January 28, 2013
Posted on January 28, 2013 at 07:01

Thanks clive ... yes there was pin conflict :)