Skip to main content
John_1992
Associate II
Sep 16, 2021 10:51 AM UTC
Question

About library of built-in bootloader

Hi,

There are host and slave MCU, both are ST MCU.

Slave MCU does not have wifi/ble for OTA upgrade. I would like to use host MCU to download slave MCU image and then use built-in bootloader to upgrade slave MCU.

I can find the communication protocol document of how to use built-in bootloader.

I would like to ask if ST has released any library of built-in bootloader for host? Or I just need to follow the protocol document to write my own library (host)?

This topic has been closed for replies.

2 replies

TDK
Sep 16, 2021 11:23 AM UTC

> I can find the communication protocol document of how to use built-in bootloader.

The general bootloader info is in AN2606.

https://www.st.com/resource/en/application_note/cd00167594-stm32-microcontroller-system-memory-boot-mode-stmicroelectronics.pdf

Specific documents exist for each protocol. For example for UART:

https://www.st.com/resource/en/application_note/cd00264342-usart-protocol-used-in-the-stm32-bootloader-stmicroelectronics.pdf

> I would like to ask if ST has released any library of built-in bootloader for host?

ST doesn't publish a library to interface with the bootloader as far as I know.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
Sep 16, 2021 4:10 PM UTC

There used to be a tool called Flash Loader Demonstrator, open source things like stm32flash, and I wrote my own years ago just following the protocol docs.

The Arduino MKR WAN 1300 boards use a Murata LoRa modules using an STM32L072, they push in a firmware update using the UART pins and BOOT0/NRST. The Atmel/Microchip processor has 1 or 2MB of space to facilitate this. There is also a pass-thru example

https://github.com/arduino-libraries/MKRWAN/tree/master/examples/MKRWANFWUpdate_standalone

https://store-usa.arduino.cc/products/arduino-mkr-wan-1300-lora-connectivity

If you don't like the ST protocol, something with better flow control like X-MODEM is an option. ST has posted there own IAP examples using Y-MODEM, and I've seen a couple of radio firmware boot-loaders implement that.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..