Skip to main content
PHolt.1
Senior
Mar 16, 2022 10:24 AM UTC
Question

32F417 to LAN8742 very slow configuration data link

Can anyone explain why there is a 1ms delay here

/**
 * @brief Disables the MAC transmission.
 * @param heth pointer to a ETH_HandleTypeDef structure that contains
 * the configuration information for ETHERNET module 
 * @retval None
 */
static void ETH_MACTransmissionDisable(ETH_HandleTypeDef *heth)
{ 
 __IO uint32_t tmpreg1 = 0U;
 
 /* Disable the MAC transmission */
 (heth->Instance)->MACCR &= ~ETH_MACCR_TE;
 
 /* Wait until the write operation will be taken into account:
 at least four TX_CLK/RX_CLK clock cycles */
 tmpreg1 = (heth->Instance)->MACCR;
 ETH_Delay(ETH_REG_WRITE_DELAY);
 (heth->Instance)->MACCR = tmpreg1;
}

I am trying to power down the LAN8742 PHY, ahead of putting the CPU in Standby. I have tried the obvious like

ETH->MACCR = 0x00008000;

but the above code snippet shows one has to then read back MACCR and write it back in after a long delay. That delay above is actually 1ms, which is way too long for my purpose.

I can see there is some sort of "USART" link along which this stuff gets sent. The 8742 data sheet describes the registers. Its SMI timing shows a max clock of ~2MHz.

This topic has been closed for replies.

11 replies

RROY.1
Associate
Jul 25, 2022 8:41 AM UTC

sir can you give me steps for hardware configure of lan8742A with stm32f429 nucleo board. I cant config that hardware.Please help me sir its too much emergency for me. my mail id is roy.rajdip1@gmail.com.please give steps how to configure.I tried static ip configure on that board.