Skip to main content
Owen Murphy
Associate
Jul 10, 2023 7:25 PM UTC
Question

10/100 Ethernet Maximum Throughput with lwIP

What is the theoretical maximum data throughput for the 10/100 Ethernet port on an MCU running lightweight IP (lwIP) on baremetal?  I am simply looking to receive UDP data and write it directly to local memory as fast as possible.  

I am using STM32H723, but I imagine that the answer will be similar for different MCU.

 

Thank you.

This topic has been closed for replies.

5 replies

LCE
Principal III
Jul 11, 2023 11:26 AM UTC

With the exact same STM32H723 I get about 90 Mbit/s transmit rate with TCP, with lwIP, bare metal.

I haven't really checked the receive rate, it was about 70 Mbit/s or so, which is far above what I need, so I didn't go into more detail.

So that's all with TCP, so you should get at least the same with UDP.

I do NOT use the ethernet HAL libraries, but from what I've read here they also reach the maximum bit rate.

Visitor II
Jul 4, 2024 9:22 AM UTC

Hello! 

 

Could you please explain a bit how to configure lwip and rtos parameters to reach that speed? I have already reach high speed on the data send, but I am not being able to receive that message on other board. I think that this may be because of the memory configuration... 

 

Thank you !!!

LCE
Principal III
Jul 4, 2024 9:45 AM UTC

I'm not using RTOS, and I'm not using the ethernet HAL drivers.

Although these high data rates should be possible with both, from what I've seen here from other users.

LCE
Principal III
Jul 11, 2023 11:29 AM UTC

For extra RAM, I recommend using the OCTOSPI with HyperRAM, works like a charm, with at least 400 Mbit/s.

QLiu.6
Associate II
Jul 25, 2023 12:59 AM UTC

Got 91-95M when runing perf on Lwip+Freertos. Board is NUCLEO-H723ZG.