Skip to main content
CParm
Associate
Nov 20, 2018 1:53 PM UTC
Question

1. What USB mode are supported by NUCLEO-F401RE which can be used to connect with PC 2. Can board connect as USB OTG? 3. NUCLEO-F401RE driver required for PC – Windows & Linux? If yes, are they available?

  1. Want to Know all the USB stack supported by NUCLEO-F401RE extra of Virtual COM port, Mass storage, Debug port?
  2. NUCLEO-F401RE does support OTG?
  3. Interrupt Transfer is supported by NUCLEO-F401RE or have any near future plan to support?
  4. Driver for NUCLEO-F401RE is available for Linux and Windows?
  5. We want to configure and read Real time data from from I2C/SPI slaves and send data to PC through USB. Do you have any such sample application?

This topic has been closed for replies.

1 reply

MZeh.1
Visitor II
Apr 21, 2020 3:15 PM UTC

Does anyone have an answer for number 4? I am also seeking Linux tools for this board. The descriptions of the downloads do not list them by OS. I am using a few different Linux types. Please post whether this is supported.