Skip to main content
CPetr.2
Associate
Sep 8, 2021 4:10 PM UTC
Solved

1.8V VDD and 3.3V IO

I am utilizing the STM32F767ZI in a design and am wondering if the following will cause any issues. I have VDD set to 1.8V so the standard IO is 1.8V, however, JTAG and USB-DFU control use 3.3V standard.

Based on the DS, the corresponding pins (PA11-14, PB3, NRST) are all FT meaning they are 5V tolerant. So, am I correct in assuming that I can use the 3.3V JTAG/USB-DFU without needing level shifters to bring them down to 1.8V?

This topic has been closed for replies.
TDK
TDKBest answer
Sep 8, 2021 4:29 PM UTC

> ... USB-DFU control use 3.3V standard.

USB has its own differential signal control. Not really equivalent to a "3.3V standard".

USB requires VDDUSB of at least 2.7V, per the datasheet. If you have VDDUSB = VDD = 1.8V, it won't work.

Not sure on JTAG.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
Sep 8, 2021 4:29 PM UTC

> ... USB-DFU control use 3.3V standard.

USB has its own differential signal control. Not really equivalent to a "3.3V standard".

USB requires VDDUSB of at least 2.7V, per the datasheet. If you have VDDUSB = VDD = 1.8V, it won't work.

Not sure on JTAG.

"If you feel a post has answered your question, please click ""Accept as Solution""."
CPetr.2
CPetr.2Author
Associate
Sep 8, 2021 6:56 PM UTC

Ah you're right, I just tested the USB-DFU and it wasn't detected below 2.2V VDD so level shifters are the way to go. Thanks!