Skip to main content
Roadrunner1805
Associate III
Feb 16, 2022 9:24 AM UTC
Solved

X-NUCLEO-LPM01A Board wrong voltage after calibration?

Hello,

I'm using the X-NUCLEO-LPM01A Board. Today I encountered a problem with the calibration. If I set the voltage to 3.3V and run a calibration I measure at VOUT only 3V. Without any calibration I measure the expected 3.3V. If I set the voltage to 1.8V and run a calibration I measure also 3V at VOUT. Without calibration it's 1.8V. Have you seen this problem? Or do I something wrong? Maybe I have to set the voltage after calibration again?

    This topic has been closed for replies.
    Roadrunner1805
    Roadrunner1805Best answer
    Associate III
    Feb 17, 2022 7:54 AM UTC

    This issue has been fixed in the new firmware version [v1.0.7] of STM32-LPM01-XN.

    Here is the link to access the last one of the firmware:

    https://www.st.com/en/development-tools/stm32-lpm01-xn.html

    2 replies

    Roadrunner1805
    Roadrunner1805AuthorBest answer
    Associate III
    Feb 17, 2022 7:54 AM UTC

    This issue has been fixed in the new firmware version [v1.0.7] of STM32-LPM01-XN.

    Here is the link to access the last one of the firmware:

    https://www.st.com/en/development-tools/stm32-lpm01-xn.html

    Peter BENSCH
    ST Technical Moderator
    Feb 17, 2022 7:56 AM UTC

    Great!

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.