Skip to main content
Visitor II
May 15, 2024
Question

writing data in flash using DMA

Hi,

I want to write data in flash using DMA. I TRIED USING 

HAL_DMA_Start() FUNCTION. DATA NOT WRITE IN FLASH. HOW TO WRITE DATA IN FLASH USING DMA IN SMT32G0B1RCT6.

 

This topic has been closed for replies.

1 reply

ST Employee
May 16, 2024

Hello,

FLASH is by default write protected so before the program will try to write to flash memory it is needed to unlock flash memory. Here is an example for STM32G0B1 which it describes:

STM32CubeG0/Projects/NUCLEO-G0B1RE/Examples/FLASH/FLASH_EraseProgram/Src/main.c at c6c0046d9278a7107261c6bf38327345df4c3efd · STMicroelectronics/STM32CubeG0 · GitHub  

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.