Skip to main content
Associate III
September 27, 2024
Question

Why is the SB9 Bridge on STM32F429I-DISC1 Not Soldered?

Hi St community,
I noticed that the SB9 bridge on the STM32F429I-DISC1, which connects the SWO pin of the ST-Link to PB3 on the STM32, is ideally not soldered by default.
Is there any specific reason for this? Does it affect the SWO functionality or debugging in any way? Should it remain unsoldered unless needed for certain configurations?
Looking forward to your insights!

Thanks!

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
September 27, 2024

Presumably, because they thought that fewer people would want to use SWO than would want to use PB3 as a normal GPIO?

 


@Shreayas_Acharaya wrote:

Does it affect the SWO functionality or debugging in any way?


With the Target's SWO output disconnected from the ST-Link, you obviously can't use the SWO feature

 


@Shreayas_Acharaya wrote:

Should it remain unsoldered unless needed for certain configurations?


If you're not going to use SWO, then there's no need to do anything - leave it unsoldered.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Karl Yamashita
Principal
September 27, 2024

SWD debugging/programming only needs SWCLK and SWDIO, so T_SWO is not needed. 

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source