Skip to main content
JKlec
Associate
May 26, 2023
Question

Why can't VDD-USB be tied to voltage derived from USB VBUS, even when VDD is OFF? If they need to be tied together, than the USB will disconnect every time VDD is OFF and will need to be re-connected. It should maintain this connection when VDD is OF

Does the STM32L072VBT6 or STM32F072VBT6 not allow for the USB connection to function, even when VDD is OFF?

This topic has been closed for replies.

1 reply

CYANG.1
ST Employee
October 25, 2023

Normally, VDD_USB is used as embeded USB PHY inside STM32. if there is no power on this power pin, USB feature won't functional.