Skip to main content
MCons.2
Associate
June 18, 2020
Question

Why can't I connect the ST-Link/V2 to my target board when the target is self-powered? (using the SWD)

If my board is not powered and the power is provided by the ST-Link, then I can program/erase all the time without issue. However for debugging it is not useful. As soon as I connect the power to the target I loose the connection.

Few things

SWDCLK and SWDIO are not used in the application

VCC is connected to ST-Link pin PIN 1 and Pin 19 thru a 10R

SWDIO is connected to ST-Link Pin 7

SWDCLK is connected to ST-Link Pin 9

GND is connected to ST-Link Pin 20

BOOT0 is pull down to GND

I did not used the ST-Link Utility, I used the STMCubeProgrammer or the STM32CubeIde.

Any clue why it does not connect to my STM32?

This topic has been closed for replies.

1 reply

Piranha
Principal III
June 20, 2020

SWDCLK and SWDIO are not used but are their configuration left intact? Using low-power modes including the the SLEEP mode has some requirements for debugging - look at DBGMCU_CR. Anyway you should connect NRST and, if required, set Connect Under Reset.