Skip to main content
CZopf.1
Visitor II
September 2, 2020
Question

Why am I getting an error: No debug probe detected in STM32 CubeProgrammer? Is there a setting in the software or is there a driver issue?

  • September 2, 2020
  • 12 replies
  • 15279 views

The STLink-V3Mini is connected to the USB port and the light on the board is green.

This topic has been closed for replies.

12 replies

Tesla DeLorean
Guru
September 2, 2020

Charging Cable?

Seeing it in Device Manager?

Open in another application? Keil?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Houda GHABRI
ST Employee
September 4, 2020

Hi @CZopf.1​ ,

Can you give us more details on the scenario used? CubeProgrammer version and board used?

best regards,

Houda

Visitor II
October 11, 2024

Am using stmcubeprogrammer v2.17.0 and the board is STM32H743IIT6

TIntr.1
Visitor II
April 19, 2021

I'm having the same problem. I've not used the STlink or programmer before. All I have done is open the programmer and connected the STlink.

Programmer: STM32CubeProgrammer v2.5.0

Official STLink-V2

Tesla DeLorean
Guru
April 19, 2021

Make sure the drivers are properly installed and the pod is seen in Device Manager

On Win7 the drivers take a while to load.

What OS are you using? What version of the Drivers are loading?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TIntr.1
Visitor II
April 20, 2021

Hi Tesla, Thanks for your reply! I'm using Mac OS High Sierra 10.13.6. Are there dedicated drivers needed for Mac?

PMars.2
Associate
August 20, 2021

I'm getting this problem both on mac and PC. I have noticed that the ST-link on my B-L4S5I-IOT01 keeps restarting and the PC loses comms. When trying to connecvt via ST-link I get "no debug probe detected" or I get "No STM32 target found"

Led state of the ST-link is inconclusive. When first plugged in takes a long time to go green. After that its pretty much a brick.

KG5ZID
Visitor II
October 1, 2021

I have a newly received Nucleo-H723ZG board. When I connect it to my Win10 PC via the ST-LINK USB port, I don't hear the usual USB connect 'jingle' nor do I see any changes in Device Manager. The board powers up ok and the blinking led demo works ok. STM32CubeProgrammer v2.6.0 also fails to see ST-LINK and reports "no debug probe detected". When I disconnect the Nucleo and connect an older ST-LINKv2 dongle, STM32CubeProgrammer sees it just fine, I get the usual USB connect jingle, and DM reports a UT-LINK usb device. I installed stsw-link0009_v2.0.2 driver but that didn't seem to change a think.

Is the Nucleo board bad? Is there a jumper that needs to be set?

KG5ZID
Visitor II
October 1, 2021

ok, nevermind. After reading a Stackoverflow article, I tried a number of different USB cables and found one that worked. It appears this Nucleo board is very picky about the usb connection. At any rate, STM32CubeProgrammer now 'sees' the board and all is well. For now.

Tesla DeLorean
Guru
October 1, 2021

MicroUSB connectors are pretty awful in nearly all manifestations. Too tight, too loose, ripping them off..

Charging cables don't have data wires, might have resistors to signal current sourcing abilities.

A lot of USB cables are very poorly made.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
KG5ZID
Visitor II
October 1, 2021

Thanks for the reply. Normally I'd agree with you and often wonder how they work at all much less after all the abuse they receive. In this case, the cables are not charge-only cables and are the same ones I use for other dev boards with micro USB connectors. They usually "just work" and I expected the Nucleo-144 to do the same. Fortunately I found the Stackoverlow post and grabbed one of my wife's old USB cords and it is working like a champ.