Skip to main content
Adam Hamilton
Senior
August 11, 2021
Solved

Where to source a 5.08mm lead pitch crystal for Nucleo-64 board

I am finding it difficult to source an external crystal for the Nucleo-64 board (The F103RB). The footprint for the X3 crystal calls for a lead pitch of 5.08mm however this seems to be very uncommon. Most of the crystals out there specifiy a lead pitch of 4.88.

Now, looking at the user guide for the Nucleo-64 boards, it mentions a part from HongKong crystal, 9SL8000016AFXHF0, which is:

  1. Not useful for me as I want to be able to use a different frequency crystal
  2. The actual datasheet for that HongKong crystal specifies the lead pitch as 4.88mm :astonished_face:

Perhaps there an updated PCB design that has not made its way into the CAD resources section of the Nucleo-64 product page for the Nucleo F103RB?

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
August 12, 2021

Hello,

As an HC-49 crystal can easily be inserted by hand on the Nucleo board, even with this 5.08mm spacing, I guess nobody really encountered a problem before.

I entered a ticket, but, the design is "old", and I don't think there will be an update.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

5 replies

TDK
August 11, 2021

The HC49 package has 4.88mm nominal lead distance with a ± 0.2mm or so tolerance. I doubt you will find nominal 5.08mm crystals, but the standard package should fit in the footprint, even if it is slightly off.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Adam Hamilton
Senior
August 11, 2021

Thank you for such a quick reply. My search also yielded nothing, except for a single oscillator with a lead pitch of 5.08mm.

As a former PCB designer, this would have been an absolute no-no for a PCB design to specify a foot print of 5.08mm and having a "she'll be right" approach.

Anyway, I would hope the ST guys out there might find some time to update the PCB footprints

Mike_ST
Mike_STBest answer
ST Technical Moderator
August 12, 2021

Hello,

As an HC-49 crystal can easily be inserted by hand on the Nucleo board, even with this 5.08mm spacing, I guess nobody really encountered a problem before.

I entered a ticket, but, the design is "old", and I don't think there will be an update.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.