Skip to main content
hansd56
Senior
June 22, 2019
Question

When is STLink/V3 Set fully implemented in STM32CubeIDE ?

Hi,

I have purchased STLink/V3 Set. I was planning to use it together with STM32CubeIDE. Unfortunately, half of the options are working. I quite like it and the speed is similar to my J-Link EDU.

  1. SWD/ST Link GDB Server not usable with 24000KHz even on a F7 and no FreeRTOS support.
  2. SWD/OpenOCD no SVW support and no FreeRTOS support from the menu.
  3. J-Link/J-Link Server SWD auto speed, inital speed option, SVW and FreeRTOS support from the STM32CubeIDE Debugger menu??

Any update would be appreciated.

This topic has been closed for replies.

1 reply

EMitu
Associate III
August 4, 2019

I've got same claim to ST-Link GDB server. It's awfully. OpenOCD works great, but SWV - still not work.