Skip to main content
LMI2
Senior III
Oct 12, 2020 5:32 PM UTC
Solved

What to do with Stlink v3 mini T_NRST pin?

I want to be absolutely sure, so should T_NRST be connected to CPU reset. (In this case STM32H750.)

This topic has been closed for replies.
TDK
TDKBest answer
Oct 12, 2020 9:19 PM UTC

The T_* prefix stands for target. It should be connected to the NRST pin of the MCU you're programming.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
TDKBest answer
Oct 12, 2020 9:19 PM UTC

The T_* prefix stands for target. It should be connected to the NRST pin of the MCU you're programming.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
Aug 7, 2024 8:33 PM UTC

I normally have NRST on MCU connected to 3.3V directly. Do I need to include a pull-down resistor if also connecting T_NRST to NRST?

 

For example,

 

3.3V — [   10k    ] —- NRST/T_NRST

 

Excuse the ASCII circuit, I’m on my phone.

LMI2
LMI2Author
Senior III
Oct 13, 2020 3:34 AM UTC

I see. The plain old reset pin. Some application notes mention also other reset signal which goes to PB4 pin. Jtag reset probably.