Skip to main content
oeliks
Associate III
August 15, 2021
Solved

What is value od HSE on nucleo L432KC?

Hi, what is the value of HSE on nucleo nano board stm32l432kc ?

​

​https://www.st.com/en/evaluation-tools/nucleo-l432kc.html#overview

​

Future : 24MHz crystall

​

But when I initialize default settings in cubemx it sets HSE as 8 MHz.​

​

Cant find value of HSE on board in board User Manual.​

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
August 15, 2021

There is no HSE crystal mounted on Nucleo-32, and also there's no OSC_OUT pin on the 'L432KC, so you cannot use a crystal for HSE with that chip.

It still has OSC_IN, so you can use an external oscillator and HSE in Bypass mode. On the Nucleo-32, you would need to connect SB17 which connects the MCO output from the on-board STLink chip ('F103) to PA0 of the target i.e. 'L432KC, and the STLink's MCO output is 8MHz.

JW

1 reply

waclawek.jan
waclawek.janBest answer
Super User
August 15, 2021

There is no HSE crystal mounted on Nucleo-32, and also there's no OSC_OUT pin on the 'L432KC, so you cannot use a crystal for HSE with that chip.

It still has OSC_IN, so you can use an external oscillator and HSE in Bypass mode. On the Nucleo-32, you would need to connect SB17 which connects the MCO output from the on-board STLink chip ('F103) to PA0 of the target i.e. 'L432KC, and the STLink's MCO output is 8MHz.

JW