Skip to main content
SRyan.2
Associate
July 9, 2022
Question

What is the specific part number used as the pin headers for nucleo 144 boards?

I want to stuff the extra connectors so that I can plug the nucleo onto a backboard, but I want to make sure that they are the same length.. I have been unable to find what appear to be compatible connectors in stock anywhere?​.

​

This has to be a frequent need but I have just been unlucky at finding the information.​

    This topic has been closed for replies.

    10 replies

    Tesla DeLorean
    Guru
    July 9, 2022

    There should be a BOM under the CAD Resources tab.

    ​

    T​he receiving pins would just be double wide 0.1" strips in a handful of lengths. Sort of stuff you can get at samtec in thru-hole or SMD forms.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    SRyan.2
    SRyan.2Author
    Associate
    July 10, 2022

    Thanks Tesla,

    I've looked through some of the BOM's but the post numbers that I found didn't seem to match the dimensions of the installed headers.

    ​

    What I am looking for is not mating pins, but the same extended post headers used on the default stuffed connectors. (Nucleo-144) comes with 4 connectors stuffed, but 2 additional outer rows that can be stuffed to expose many more signals. ​I would like to find matching connectors so the pins out the bottom all contact at the same point and the headers on the top all share the same plane and have matching contact points. We are using these in some test fixtures for inhouse designed STM32 parts and want to make things as simple as possible.

    FThie.1
    Visitor II
    July 10, 2022

    I looked on my Nucleo L5 BOM ( https://www.st.com/resource/en/bill_of_materials/mb1361_bom.zip )

    and found some Samtec SSW-1xx-23-x-D.

    The datasheet is here: https://suddendocs.samtec.com/catalog_english/ssw_th.pdf

    and the "23" in the part reference indicates some low insertion force 10mm pins

    Karl Yamashita
    Principal
    February 11, 2025

    Are you looking for connectors with the female/male connectors like the Arduino connectors? Or some male/female SIP headers for the morpho connection pins?

    If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
    JMerk.1
    Associate
    February 11, 2025

    The NUCLEO-144 pin boards do not have the CN11 and CN12 morpho connectors populated.  I have been looking for parts to populate these "missing connectors".  I really like the morpho pins on the Nucleo-64 boards, allowing me to connect parts to the top side and attach instruments to the bottom side of the board.  The BOM for the Nucleo-64 boards indicates a "Lyconn 313238S161185", but this part is hard to locate.  The Samtec TSW-135-09-G-D appears to be a close match.

    Tesla DeLorean
    Guru
    February 11, 2025

    The 38 pin 2x19 aren't a popular format, ie non-stock / special-order

    Pololu had TI-RSLK MAX headers  https://www.pololu.com/product/3676

    https://www.pololu.com/category/240/ti-robotics-system-learning-kit-max-ti-rslk-max-parts-and-accessories

    I've used these for fixturing QSPI Flash adapters, etc.

    The Arduino Mega 36 pin 2x18 can be staggered in a pinch, and have higher availability.

    The unpopulated headers on the NUCLEO-144's likely aim for direct wire soldering, or 0.1" pitch socket/headering of your choosing, I'm guessing not populated due to high BoM costs, and the mating/removal forces being quite high.

    Amazon often has assorted options, including some break-to-length sockets and headers

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..