Skip to main content
CGand.1
Associate
February 18, 2020
Question

What is the correct recommended pad size for the STM32 in the TFBGA240+25? The Table 135 of the datasheet seems incorrect.

With a ball size of 0.4mm I would expect a pad size of 0.36mm , but 0.225 mm is in the table.

This topic has been closed for replies.

3 replies

ST Technical Moderator
February 25, 2020

Hello @CGand.1​ ,

Which H7 Datasheet ? Please point to the latest Datasheet.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
CGand.1
CGand.1Author
Associate
February 25, 2020
ST Technical Moderator
February 25, 2020

 Hi @CGand,

You are right, the PCB recommended design rules for TFBGA240+25 (0.8mm) pitch is not correct.

The values should be:

  • Pitch : 0.8
  • Dpad : 0.400 mm
  • DSM : 0.500 mm
  • Stencil opening : 0.400mm

I raised this internally for correction in the next STM32H7 datasheets.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks