Skip to main content
EDağl.1
Associate
April 18, 2023
Solved

What is the correct power supply circuit of PL2303 UART Brigde with STM32F407VG (Discovery)

At first, I'm an absolute beginner, I'm still on my way to learn more about STM family regarding electronics.

Lately I've been having circuit issues with PL2303. After reading datasheet, number 6.2,

5V can also be used as input power supplies

I've connected my PL2303's 5V to STM32's 5V but after a while, my STM32 had some damage and it close-circuited 5V and GND. Same thing happened after I had my new STM32 and connecting the PL2303's 5V to STM32's VDD.

I'm dead sure about the cabling and soldering and there's nothing wrong with it.

I'd be so appreciated to hear some ideas about it.

Thanks!

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
April 18, 2023

I'd jumper it at 3.3V is supposed to be the VCCIO, the IO level the USB Serial uses to the STM32 UART pins.

You don't need to connect the VCC to the STM32

Connect the GND, so the circuits are common, connect the TX of the dongle to the UART-RX on the STM32 side. And the STM32 UART-TX to the RX of the dongle.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
April 18, 2023

I'd jumper it at 3.3V is supposed to be the VCCIO, the IO level the USB Serial uses to the STM32 UART pins.

You don't need to connect the VCC to the STM32

Connect the GND, so the circuits are common, connect the TX of the dongle to the UART-RX on the STM32 side. And the STM32 UART-TX to the RX of the dongle.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
EDağl.1
EDağl.1Author
Associate
April 18, 2023

So at the end, VCCIO pin of the PL2023 has to be empty and only GND, RXD and TXD has to be connected to the STM32. Am I right?

Tesla DeLorean
Guru
April 18, 2023

Or you remove the Jumper, and provide the IO level to use from the STM32 side.

Akin to IOREF on the Arduino rail,.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..