Skip to main content
ALisk.1
Associate
April 20, 2021
Question

What are the design criteria for Nucleo Oscillator?

What are the design criteria by which the oscillator for the Nucleo dev kits has been selected?

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
April 20, 2021

Cheapness? The BOM call out the exact part numbers if you want to know the ppm, temp range, and load capacitance..

There are literally dozens of "Nucleo" boards, including 32, 64 and 144-pin formats. Can you perhaps narrow the question a little?

There is an Application Note on Crystal selection, and component values.

The NUCLEO's include an ST-LINK/V2 connecting via USB, USB places accuracy expectations on the clocking.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ALisk.1
ALisk.1Author
Associate
April 20, 2021
To be clearer:
Is there a specific reason that ST selected the NX3225GD for Nucleo 144pin?
Price?
Stability?
ESR?
Tolerance?
etc..
Thanks
ST Technical Moderator
April 20, 2021

Hello @ALisk.1​ and welcome to the STM32 Community,

I recommend you this AN2867 Application note Oscillator design guide for STM8AF/AL/S, STM32 MCUs and MPUs, it provides guidelines for the oscillator design. 

When your question is answered, please close this topic by choosing "Select as Best".

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks