Skip to main content
KPate.61
Associate
July 1, 2022
Solved

Virtual com port driver not properly installed

ST Link V3 SET is giving error due to virtual com port not installed in computer

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
July 22, 2022

Hi @KPate.6​ ,

A similar question is already asked here.

In the description of the STSW-STM32102 you can find:

Virtual COM Port driver installation package for Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x.

Windows 10 does not require the installation of the Virtual COM Port driver anymore, as it is already built in.

So, if you use a Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x try to uninstall the driver and reinstall the last version.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

1 reply

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
July 22, 2022

Hi @KPate.6​ ,

A similar question is already asked here.

In the description of the STSW-STM32102 you can find:

Virtual COM Port driver installation package for Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x.

Windows 10 does not require the installation of the Virtual COM Port driver anymore, as it is already built in.

So, if you use a Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x try to uninstall the driver and reinstall the last version.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.