Skip to main content
Visitor II
Jul 9, 2025 11:14 AM UTC
Question

video camera module connection to STM32H745-Disco

we need to connect a camera to the STM32H745-Disco board. Our ultimate goal is to develop an application similar to the image_classification example from the STM32AI Model Zoo. Since we are unable to purchase another board, we would like to ask if it is possible to connect a camera module to the STM32H745-Disco for this purpose. Any guidance or suggestions would be greatly appreciated.

This topic has been closed for replies.

1 reply

QSHAO.1
ST Employee
Jul 10, 2025 7:41 AM UTC

As no camera connector available on STM32H745-Disco board, even DCMI interface is supported by STM32H745XI on this board, I think it may not possible to connect it to a camera module or very complex to do it.