Skip to main content
FZher.1665
Associate
Nov 14, 2019 1:15 PM UTC
Solved

V1.1.0, segger j-link support gone?

Hi I installed STM32CubeIDE V1.1.0 and now I can't select J-Link as a debug probe, only ST-link (GDB & OpenOCD).

I get the J-link if the project was created in an older STM32CubeIDE version, but not in the new 1.1.0.

Any hints on how to enable J-link?

This topic has been closed for replies.
Markus GIRDLAND
Markus GIRDLANDBest answer
ST Employee
Nov 27, 2019 8:59 AM UTC

The internal weekly build we do has fixed this so you will be able to use J-link in the next version of CubeIDE. I've tested it myself and now there's a pop-up warning that there's no support if you would choose a dual-core H7 with J-link (or some other incompatible probe and target) instead of filtering.

12 replies

BillR
Associate III
Nov 14, 2019 3:49 PM UTC

Sorry I don't have a solution for you but I am having the same problem. In my case I fortunately had an STLink V2 laying around which is working fine for me. It might be a little slower to load but fine for at least general debugging so far. Also at $29 vs hundreds for the JLink I think they are a bargain.

Cartu38 OpenDev
Graduate II
Nov 14, 2019 6:20 PM UTC

Which target are you working with ?

FZher.1665
Associate
Nov 15, 2019 6:54 AM UTC

@BillR​ I have one to, but I want to use System View from Segger to debug FreeRTOS. Its nice to have unlimited break points and better speed as well.

@Cartu38 OpenDev​  I use STM32H753.

@Markus GIRDLAND​ Is there any solution or workaround?

Markus GIRDLAND
ST Employee
Nov 15, 2019 9:52 AM UTC

The J-link option is disabled on all H7 devices. This is because the dual-core H7 devices does not have J-link support. However, this gets the negative side-effect that single core H7 devices gets blocked as well.

I don't believe there's a workaround but I know the debate about whether to block these devices or not is still ongoing so I will lift this thread as an example of negative consequences that can come from this.

FZher.1665
Associate
Nov 15, 2019 10:11 AM UTC

Please do so

After reading the release note in V1.1.0 that SEGGER is supported, we bout a J-link only for this..

Cartu38 OpenDev
Graduate II
Nov 15, 2019 8:38 AM UTC

I confirm STM32H753 sounds locked on my side too.

Pavel A.
Nov 27, 2019 1:09 AM UTC

How J-Link does unlimited breakpoints? IIRC number of breakpoints is limitation of the MCU, not of the debugger dongle?

-- pa

Uwe Bonnes
Chief
Nov 27, 2019 10:11 AM UTC

The reflash the flash sector where the breakpoint resides.