Skip to main content
BSANT.17
Associate II
May 13, 2020
Question

Use STLink V3 as RS485 VCP

I would like to plug RS485 on VCP STLINKV3. I try to plug RTS (VPC2) on DE, but I finally saw on that RTS/CTS cannot be controled by software... Can we plug DE by an other way ?

I would you like to try GPIO control, do you have simple CLI or GUI ?

Regards,

This topic has been closed for replies.

3 replies

TDK
May 14, 2020

What is "DE"?

You will need a hardware level shifter to convert between RS485 and the single-ended 0-3.3V levels the ST-Link UART is expecting. And it doesn't support hardware data control. I don't believe the ST-Link exposes any GPIO pins for general use. Could be wrong.

"If you feel a post has answered your question, please click ""Accept as Solution""."
BSANT.17
BSANT.17Author
Associate II
May 14, 2020

On ST3485EBDR DE pin permit to send data.

ST-Link V3 provides 4 gpio, 1 uart, 1 uart+flow control, can, spi, I2C....

S.Ma
Principal
May 14, 2020

Is USART full duplex and RS485 half duplex?

Conversion maynot be so trivial.