Skip to main content
PSchb.1
Associate II
Mar 24, 2022 9:24 AM UTC
Solved

USART3 (on Arduino connector CN14) troubles on stm32u5 iot eval board BU585IIO2A

i'm using the  stm32u5 iot eval board BU585IIO2A and want to use USART3 on Arduino connector CN14

i successfully got the PWM working on PIN7 of CN14 but i fail to get anything sent / received on UASRT3 (Pins 1 and 2 of CN14)

are there any hints / samples how to get this working ?

thx, peter

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
Mar 25, 2022 1:37 PM UTC

Yes, that should be the problem...

In the .ioc you have to assign it to PD8/PD9,

and you should end up with that:

   /* Peripheral clock enable */

   __HAL_RCC_USART3_CLK_ENABLE();

   __HAL_RCC_GPIOD_CLK_ENABLE();

   /**USART3 GPIO Configuration

   PD8    ------> USART3_TX

   PD9    ------> USART3_RX

   */

   GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;

   GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

   GPIO_InitStruct.Pull = GPIO_NOPULL;

   GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

   GPIO_InitStruct.Alternate = GPIO_AF7_USART3;

   HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

/* USART3 interrupt Init */

HAL_NVIC_SetPriority(USART3_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(USART3_IRQn);

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

13 replies

Mike_ST
ST Technical Moderator
Mar 24, 2022 4:08 PM UTC

Hello,

USART3 is connected to STMOD+ connector as well through the U3 switch, as shown in schematic page 7.

So, please make sure that PH15 (STMOD+.UART3_SPI3_SEL) is set to Output Low.

Maybe that is the problem.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
PSchb.1
PSchb.1Author
Associate II
Mar 24, 2022 4:47 PM UTC

thx for your quick response.

actually, in the specs it reads that PH15 has to be set to HIGH and i did that.(page 35 PH15 set high)

which spec are you referring to ? (mine is : um2839-discovery-kit-for-iot-node-with-stm32u5-series-stmicroelectronics.pdf)

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOH, GPIO_PIN_15, GPIO_PIN_SET);

best regards, peter

Mike_ST
ST Technical Moderator
Mar 24, 2022 5:04 PM UTC

I'm refering to the schematic:

https://www.st.com/resource/en/schematic_pack/mb1551-u585i-c02_schematic.pdf

Page 35 of the UM2839 user's manual explains how to use the USART3 on the STMOD+ CN2 connector, not on the Arduino connector.

In your case, you don't want the U3 switch to drive the USART3 lines.

So you have to set U3 to drive the SPI lines so it it won't disturb USART3 lines.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
PSchb.1
PSchb.1Author
Associate II
Mar 25, 2022 9:10 AM UTC

i really appriciate your support !

but it does not work for me and i still don't know why.

so, i tried it both ways , this way

HAL_GPIO_WritePin(GPIOH, GPIO_PIN_15, GPIO_PIN_RESET);

and this way

HAL_GPIO_WritePin(GPIOH, GPIO_PIN_15, GPIO_PIN_SET);

both ways do not work.

do you know the reason why ? what am i missing ?

how SHOULD it be set ? and when: just before MX_USART3_UART_Init(); or before using uart e.g with HAL_UART_Transmit(&huart3, "peter\r\n", 7, 10);

i made a small test project just for testing that UART3 on Arduino connector CN14 : should you send you the main.c ?

thx, again,

peter

Mike_ST
ST Technical Moderator
Mar 25, 2022 10:00 AM UTC

Here is mine instead, tested using a USB <-> serial converter on the CN14 connector.

Hope that helps.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Mike_ST
Mike_STBest answer
ST Technical Moderator
Mar 25, 2022 1:37 PM UTC

Yes, that should be the problem...

In the .ioc you have to assign it to PD8/PD9,

and you should end up with that:

   /* Peripheral clock enable */

   __HAL_RCC_USART3_CLK_ENABLE();

   __HAL_RCC_GPIOD_CLK_ENABLE();

   /**USART3 GPIO Configuration

   PD8    ------> USART3_TX

   PD9    ------> USART3_RX

   */

   GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;

   GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

   GPIO_InitStruct.Pull = GPIO_NOPULL;

   GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

   GPIO_InitStruct.Alternate = GPIO_AF7_USART3;

   HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

/* USART3 interrupt Init */

HAL_NVIC_SetPriority(USART3_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(USART3_IRQn);

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.