Skip to main content
Associate III
December 3, 2023
Solved

Unable to load to Nucleo board

Scenario:

Windows 11 connected to Nucleo-L476RG.
Fresh install of STMCubeIDE
Version: 1.14.0
Build: 19471_20231121_1200 (UTC)
OS: Windows 11, v.10.0, x86_64 / win32

Ran STLinkUpgrade 3.13.4
Result: Update to Firmware: V2J43M28 STM Debug+Mass storage+VCP Upgrade successful.

File > New STM Project
Selected board L476RG
Project name testtest
Initialised all peripherals with default.

Configurator opened main.c
Project > Build Project
11:30:19 Build Finished. 0 errors, 0 warnings. (took 3s.143ms)

Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (0) Unknown. Please check power and cabling to target.

Failed to bind to port 61235, error code -1: No error
Failure starting SWV server on TCP port: 61235
Failed to bind to port 61234, error code -1: No error
Failure starting GDB server: TCP port 61234 not available.
Shutting down...
Exit.

My question:

The cable is a known good one, and the STLink upgrade was successful, so it seems to me that there is nothing wrong with

 

This topic has been closed for replies.
DabboBest answer
Associate III
December 3, 2023

Solved! And I think I know what the problem might be.

From the Windows "Add & Remove Programs" menu I removed anything with ST in the name and did another fresh installation. This time I got the message "Do you want to allow public and private networks to access this app? Windows Firewall has blocked some features of st-link_gdbserver.exe on all public and private networks".

I have not seen this message before.

I clicked "Allow" and the installation continued, and now it works.

Another Sunday wasted - ho-hum

ADDED LATER: on reflection, in the process of uninstalling I uninstalled 2 versions of STMCubeIDE as well as one STLink file. It's possible the problem was related to that, as per the links above. Either way, a complete uninstall / reinstall fixed it

3 replies

DabboAuthor
Associate III
December 3, 2023

By the way, I know both my Nucleo board and the cable are good as they work on my Linux machine

STTwo-32
ST Technical Moderator
December 3, 2023

Hello @Dabbo 

I suggest you to take a look at this post. It may be helpful.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DabboAuthorBest answer
Associate III
December 3, 2023

Solved! And I think I know what the problem might be.

From the Windows "Add & Remove Programs" menu I removed anything with ST in the name and did another fresh installation. This time I got the message "Do you want to allow public and private networks to access this app? Windows Firewall has blocked some features of st-link_gdbserver.exe on all public and private networks".

I have not seen this message before.

I clicked "Allow" and the installation continued, and now it works.

Another Sunday wasted - ho-hum

ADDED LATER: on reflection, in the process of uninstalling I uninstalled 2 versions of STMCubeIDE as well as one STLink file. It's possible the problem was related to that, as per the links above. Either way, a complete uninstall / reinstall fixed it